<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックS32K344 MBDT UART</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K344-MBDT-UART/m-p/1909445#M9304</link>
    <description>&lt;P&gt;Hello Community,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I was working on UART example&amp;nbsp;s32k3xx_uart_async_s32ct, the example is working for only 1 character like 'H'. I want communication with multiple character like 'Hello'. Please suggest the changes in Simulink or provide example model for the reference.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 16 Jul 2024 06:34:50 GMT</pubDate>
    <dc:creator>avinashstarkenn</dc:creator>
    <dc:date>2024-07-16T06:34:50Z</dc:date>
    <item>
      <title>S32K344 MBDT UART</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K344-MBDT-UART/m-p/1909445#M9304</link>
      <description>&lt;P&gt;Hello Community,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I was working on UART example&amp;nbsp;s32k3xx_uart_async_s32ct, the example is working for only 1 character like 'H'. I want communication with multiple character like 'Hello'. Please suggest the changes in Simulink or provide example model for the reference.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 16 Jul 2024 06:34:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K344-MBDT-UART/m-p/1909445#M9304</guid>
      <dc:creator>avinashstarkenn</dc:creator>
      <dc:date>2024-07-16T06:34:50Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 MBDT UART</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K344-MBDT-UART/m-p/1910533#M9307</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/221165"&gt;@avinashstarkenn&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The mentioned model (&lt;SPAN&gt;s32k3xx_uart_async_s32ct&lt;/SPAN&gt;) is indeed a loopback example, showcasing an application that is sending back, via UART, the input from the keyboard.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If you would like to implement a more complex scenario,&amp;nbsp;I suggest you take a look at the following examples delivered in the toolbox:&lt;/P&gt;
&lt;P&gt;-&amp;nbsp;&lt;STRONG&gt;s32k3xx_uart_leds_ebt /&amp;nbsp;s32k3xx_uart_leds_s32ct&lt;/STRONG&gt; from the &lt;STRONG&gt;demos&lt;/STRONG&gt; folder, which illustrates how to combine UART and DIO functionalities to control the LEDs on the board using UART. Based on the keyboard input pressed (R, G, B, or SPACE), the corresponding LED will be toggled and a specific message will be sent via UART. Additionally, you could activate or deactivate all the LEDs on the board by pressing USER_SW0 or USER_SW1, and a specific text will be displayed via UART.&lt;/P&gt;
&lt;P&gt;-&amp;nbsp;&lt;STRONG&gt;s32k3xx_icu_signal_edge_detect_ebt&lt;/STRONG&gt; from the &lt;STRONG&gt;icu&lt;/STRONG&gt; folder, which uses UART to display the signal edges of a generated signal, and the activation condition changes. Based on the switch pressed, it will be displayed via UART specific messages.&lt;/P&gt;
&lt;P&gt;I hope the above examples could be a starting point for your application.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Dragos&lt;/P&gt;</description>
      <pubDate>Wed, 17 Jul 2024 10:29:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K344-MBDT-UART/m-p/1910533#M9307</guid>
      <dc:creator>dragostoma</dc:creator>
      <dc:date>2024-07-17T10:29:37Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 MBDT UART</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K344-MBDT-UART/m-p/1916124#M9322</link>
      <description>Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/199423"&gt;@dragostoma&lt;/a&gt;,&lt;BR /&gt;The solution that you gave are not related to the question that I have asked.&lt;BR /&gt;I want a model where I want to send and receive multiple string(like 'Hello' and not a single character like only 'H').We want to view that string.</description>
      <pubDate>Wed, 24 Jul 2024 12:02:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K344-MBDT-UART/m-p/1916124#M9322</guid>
      <dc:creator>avinashstarkenn</dc:creator>
      <dc:date>2024-07-24T12:02:06Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 MBDT UART</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K344-MBDT-UART/m-p/1916167#M9323</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/221165"&gt;@avinashstarkenn&lt;/a&gt; ,&lt;/P&gt;
&lt;P&gt;A better solution for your application in this case could be the&amp;nbsp;&lt;STRONG&gt;s32k3xx_uart_buffer_s32ct&lt;/STRONG&gt; model example which shows how to use UART component to transfer data of variable length using a circular buffer. You should type characters in the terminal and a correct run of the program will write back those characters to the terminal when the ENTER key is pressed. I recommend using this model as a starting point for your application.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope this helps,&lt;/P&gt;
&lt;P&gt;Dragos&lt;/P&gt;</description>
      <pubDate>Wed, 24 Jul 2024 12:46:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K344-MBDT-UART/m-p/1916167#M9323</guid>
      <dc:creator>dragostoma</dc:creator>
      <dc:date>2024-07-24T12:46:51Z</dc:date>
    </item>
  </channel>
</rss>