<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K344 Variables turning into nan in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K344-Variables-turning-into-nan/m-p/1895971#M9276</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm using the S32K344 Q172&amp;nbsp;&lt;A href="https://www.nxp.com/products/no-longer-manufactured/s32k3x4-q172-general-purpose-development-board:S32K3X4EVB-Q172" target="_self"&gt;EVB&lt;/A&gt;&amp;nbsp;in an inverter application, in which it's hosting a custom FOC algorithm.&lt;BR /&gt;It is communicating via the CAN bus with a MicroAutobox II that is hosting a virtual model of an inverter and a PMSM.&lt;/P&gt;&lt;P&gt;The FOC algorithm was designed on Simulink using the S32K Model Based Designe toolbox v1.4 and simulink libraries and then it was tested with a virtual model of a PMSM and it's inverter.&lt;/P&gt;&lt;P&gt;After flashing the FOC algorithm onto the&amp;nbsp;S32K344 Q172 and initiating communication with the&amp;nbsp;MicroAutobox II I can follow the evolution of variables using freemaster.&lt;/P&gt;&lt;P&gt;Even though I used saturation blocks, I can see some variables that grow bigger and bigger until they become nan.&lt;/P&gt;&lt;P&gt;How can I fix this issue?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
    <pubDate>Fri, 28 Jun 2024 14:18:19 GMT</pubDate>
    <dc:creator>REM</dc:creator>
    <dc:date>2024-06-28T14:18:19Z</dc:date>
    <item>
      <title>S32K344 Variables turning into nan</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K344-Variables-turning-into-nan/m-p/1895971#M9276</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm using the S32K344 Q172&amp;nbsp;&lt;A href="https://www.nxp.com/products/no-longer-manufactured/s32k3x4-q172-general-purpose-development-board:S32K3X4EVB-Q172" target="_self"&gt;EVB&lt;/A&gt;&amp;nbsp;in an inverter application, in which it's hosting a custom FOC algorithm.&lt;BR /&gt;It is communicating via the CAN bus with a MicroAutobox II that is hosting a virtual model of an inverter and a PMSM.&lt;/P&gt;&lt;P&gt;The FOC algorithm was designed on Simulink using the S32K Model Based Designe toolbox v1.4 and simulink libraries and then it was tested with a virtual model of a PMSM and it's inverter.&lt;/P&gt;&lt;P&gt;After flashing the FOC algorithm onto the&amp;nbsp;S32K344 Q172 and initiating communication with the&amp;nbsp;MicroAutobox II I can follow the evolution of variables using freemaster.&lt;/P&gt;&lt;P&gt;Even though I used saturation blocks, I can see some variables that grow bigger and bigger until they become nan.&lt;/P&gt;&lt;P&gt;How can I fix this issue?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
      <pubDate>Fri, 28 Jun 2024 14:18:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K344-Variables-turning-into-nan/m-p/1895971#M9276</guid>
      <dc:creator>REM</dc:creator>
      <dc:date>2024-06-28T14:18:19Z</dc:date>
    </item>
  </channel>
</rss>