<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Not able to flash Code  in board s32k148 in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Not-able-to-flash-Code-in-board-s32k148/m-p/1888408#M9224</link>
    <description>&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;I am not able to flash the board. The green led (D10) keeps blinking rapidly when I start to flash the Board through NXP MBD toolbox using MATLAB. Before this issue, everything was working fine. I was able to flash the board using MBD toolbox as well as using the S32 Design Studio. I have checked in one NXP community forum that this action of LED (D10) occurs when there is any error. Further more no specific information was provided regarding the error. The LED (D10) blinks rapidly for 8 time and then gets OFF for 2 seconds, this action takes place repeatedly whenever I try to flash the program.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;Even I'm trying to flash RBF image but same happening it is not able to flash in s32k148 just reset green led&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 17 Jun 2024 06:38:51 GMT</pubDate>
    <dc:creator>saurabhkulkarni123</dc:creator>
    <dc:date>2024-06-17T06:38:51Z</dc:date>
    <item>
      <title>Not able to flash Code  in board s32k148</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Not-able-to-flash-Code-in-board-s32k148/m-p/1888408#M9224</link>
      <description>&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;I am not able to flash the board. The green led (D10) keeps blinking rapidly when I start to flash the Board through NXP MBD toolbox using MATLAB. Before this issue, everything was working fine. I was able to flash the board using MBD toolbox as well as using the S32 Design Studio. I have checked in one NXP community forum that this action of LED (D10) occurs when there is any error. Further more no specific information was provided regarding the error. The LED (D10) blinks rapidly for 8 time and then gets OFF for 2 seconds, this action takes place repeatedly whenever I try to flash the program.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;Even I'm trying to flash RBF image but same happening it is not able to flash in s32k148 just reset green led&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 17 Jun 2024 06:38:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Not-able-to-flash-Code-in-board-s32k148/m-p/1888408#M9224</guid>
      <dc:creator>saurabhkulkarni123</dc:creator>
      <dc:date>2024-06-17T06:38:51Z</dc:date>
    </item>
    <item>
      <title>Re: Not able to flash Code  in board s32k148</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Not-able-to-flash-Code-in-board-s32k148/m-p/1890220#M9228</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/202837"&gt;@saurabhkulkarni123&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If my assumption is correct you may need to update or reflash the firmware of the onboard OpenSDA device for the S32K148. A tutorial for such process has been described previously in this community page&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Update-OpenSDA-Firmware-on-EVB/ta-p/1111067" target="_blank"&gt;https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Update-OpenSDA-Firmware-on-EVB/ta-p/1111067&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please apply the septs described in there for your type of board.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Marius&lt;/P&gt;</description>
      <pubDate>Wed, 19 Jun 2024 08:51:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Not-able-to-flash-Code-in-board-s32k148/m-p/1890220#M9228</guid>
      <dc:creator>mariuslucianand</dc:creator>
      <dc:date>2024-06-19T08:51:29Z</dc:date>
    </item>
  </channel>
</rss>