<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックRe: .bin file not created for PIL, but code built correctly into .elf, seems something missing from</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/bin-file-not-created-for-PIL-but-code-built-correctly-into-elf/m-p/1887856#M9206</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;The .bin file is not missing it is still created from the .elf file, like you mentioned, but in a subfolder not at the same level as the model.&lt;BR /&gt;As far as I know the problem occurs when the selected download method is not "USB Multilink/Embedded Debugger - JTAG".&lt;BR /&gt;&lt;BR /&gt;The problem is fixed in the "MBDT 1.5 for the S32K3xx series" toolbox release.&lt;/P&gt;</description>
    <pubDate>Fri, 14 Jun 2024 11:30:03 GMT</pubDate>
    <dc:creator>Adrian_Gherca</dc:creator>
    <dc:date>2024-06-14T11:30:03Z</dc:date>
    <item>
      <title>.bin file not created for PIL, but code built correctly into .elf, seems something missing from make</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/bin-file-not-created-for-PIL-but-code-built-correctly-into-elf/m-p/1886260#M9197</link>
      <description>&lt;P&gt;i have a model that if i generate code for it as a top model in external mode it builds, downloads and runs. when i try to include the same model as a PIL from a higher level model, the code builds a .elf, but it seems the make file is missing a post build call to convert the .elf to a .bin when in PIL mode.&lt;/P&gt;&lt;P&gt;one screenshot is the error message when in PIL mode, the other shows the step in external mode where the .bin is created from the .elf&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jun 2024 14:52:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/bin-file-not-created-for-PIL-but-code-built-correctly-into-elf/m-p/1886260#M9197</guid>
      <dc:creator>Deskwork4130</dc:creator>
      <dc:date>2024-06-12T14:52:58Z</dc:date>
    </item>
    <item>
      <title>Re: .bin file not created for PIL, but code built correctly into .elf, seems something missing from</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/bin-file-not-created-for-PIL-but-code-built-correctly-into-elf/m-p/1886262#M9198</link>
      <description>&lt;P&gt;maybe directory setting related? it does seem to be getting generated.&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;"### Invoking postbuild tool "ELF To Binary Converter" ..."&lt;BR /&gt;arm-none-eabi-objcopy -O binary ./HEC_Prototype.elf ../../../../HEC_Prototype.bin&lt;BR /&gt;"### Done invoking postbuild tool."&lt;BR /&gt;"### Successfully generated all binary outputs."&lt;/P&gt;&lt;/BLOCKQUOTE&gt;</description>
      <pubDate>Wed, 12 Jun 2024 15:02:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/bin-file-not-created-for-PIL-but-code-built-correctly-into-elf/m-p/1886262#M9198</guid>
      <dc:creator>Deskwork4130</dc:creator>
      <dc:date>2024-06-12T15:02:02Z</dc:date>
    </item>
    <item>
      <title>Re: .bin file not created for PIL, but code built correctly into .elf, seems something missing from</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/bin-file-not-created-for-PIL-but-code-built-correctly-into-elf/m-p/1886264#M9199</link>
      <description>&lt;P&gt;i verified that if i manually copy the .bin to the same directory as the .elf it works. so what do i need to change so that the .bin is generated in the desired folder?&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jun 2024 15:09:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/bin-file-not-created-for-PIL-but-code-built-correctly-into-elf/m-p/1886264#M9199</guid>
      <dc:creator>Deskwork4130</dc:creator>
      <dc:date>2024-06-12T15:09:15Z</dc:date>
    </item>
    <item>
      <title>Re: .bin file not created for PIL, but code built correctly into .elf, seems something missing from</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/bin-file-not-created-for-PIL-but-code-built-correctly-into-elf/m-p/1887856#M9206</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;The .bin file is not missing it is still created from the .elf file, like you mentioned, but in a subfolder not at the same level as the model.&lt;BR /&gt;As far as I know the problem occurs when the selected download method is not "USB Multilink/Embedded Debugger - JTAG".&lt;BR /&gt;&lt;BR /&gt;The problem is fixed in the "MBDT 1.5 for the S32K3xx series" toolbox release.&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jun 2024 11:30:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/bin-file-not-created-for-PIL-but-code-built-correctly-into-elf/m-p/1887856#M9206</guid>
      <dc:creator>Adrian_Gherca</dc:creator>
      <dc:date>2024-06-14T11:30:03Z</dc:date>
    </item>
    <item>
      <title>Re: .bin file not created for PIL, but code built correctly into .elf, seems something missing from</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/bin-file-not-created-for-PIL-but-code-built-correctly-into-elf/m-p/1887890#M9208</link>
      <description>&lt;P&gt;Unfortunately I cannot provide a solution for a local fix. In the latest toolbox release this error doesn't occur anymore.&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jun 2024 12:15:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/bin-file-not-created-for-PIL-but-code-built-correctly-into-elf/m-p/1887890#M9208</guid>
      <dc:creator>Adrian_Gherca</dc:creator>
      <dc:date>2024-06-14T12:15:56Z</dc:date>
    </item>
  </channel>
</rss>