<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックS32K1XX MBDT SPI clock settings help</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K1XX-MBDT-SPI-clock-settings-help/m-p/1879642#M9163</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;I am trying to communicate and configure a TLE8718SA Lowside Switch through SPI communication. In the documentation of that IC it is mentioned that the clock signal has to be continous yet I do not see such an option in the LPSPI configuration block. Is there a way I could manually force the clock signal to be continous?&lt;BR /&gt;&lt;BR /&gt;Cheers&lt;/P&gt;</description>
    <pubDate>Fri, 07 Jun 2024 07:36:12 GMT</pubDate>
    <dc:creator>ErwinR</dc:creator>
    <dc:date>2024-06-07T07:36:12Z</dc:date>
    <item>
      <title>S32K1XX MBDT SPI clock settings help</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K1XX-MBDT-SPI-clock-settings-help/m-p/1879642#M9163</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;I am trying to communicate and configure a TLE8718SA Lowside Switch through SPI communication. In the documentation of that IC it is mentioned that the clock signal has to be continous yet I do not see such an option in the LPSPI configuration block. Is there a way I could manually force the clock signal to be continous?&lt;BR /&gt;&lt;BR /&gt;Cheers&lt;/P&gt;</description>
      <pubDate>Fri, 07 Jun 2024 07:36:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K1XX-MBDT-SPI-clock-settings-help/m-p/1879642#M9163</guid>
      <dc:creator>ErwinR</dc:creator>
      <dc:date>2024-06-07T07:36:12Z</dc:date>
    </item>
  </channel>
</rss>