<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Error conversion of voltage drops of NTC sensors to temperature in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Error-conversion-of-voltage-drops-of-NTC-sensors-to-temperature/m-p/1863395#M9075</link>
    <description>&lt;P&gt;&lt;SPAN&gt;The MC33772C BMS slaves are connected to the S32K144EVB evaluation board via TPL lines. I program the evaluation board using the Model-Based Design Toolbox from NXP in Simulink. NTC sensors are mounted on the MC33772C, and I need to read the temperatures measured by the evaluation board. However, the temperature conversions are incorrect. The analog voltages from the GPIOs of the MC33772C are correct, so I believe the issue lies with the conversion process. The conversion parameters, such as the NTC fixed resistance and NTC reference resistance, are correctly set. I tried configuring the GPIOs as ratiometric analog inputs, but the temperature conversions are still incorrect. I can't determine the cause of the problem.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 10 May 2024 11:01:03 GMT</pubDate>
    <dc:creator>URC</dc:creator>
    <dc:date>2024-05-10T11:01:03Z</dc:date>
    <item>
      <title>Error conversion of voltage drops of NTC sensors to temperature</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Error-conversion-of-voltage-drops-of-NTC-sensors-to-temperature/m-p/1863395#M9075</link>
      <description>&lt;P&gt;&lt;SPAN&gt;The MC33772C BMS slaves are connected to the S32K144EVB evaluation board via TPL lines. I program the evaluation board using the Model-Based Design Toolbox from NXP in Simulink. NTC sensors are mounted on the MC33772C, and I need to read the temperatures measured by the evaluation board. However, the temperature conversions are incorrect. The analog voltages from the GPIOs of the MC33772C are correct, so I believe the issue lies with the conversion process. The conversion parameters, such as the NTC fixed resistance and NTC reference resistance, are correctly set. I tried configuring the GPIOs as ratiometric analog inputs, but the temperature conversions are still incorrect. I can't determine the cause of the problem.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 10 May 2024 11:01:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Error-conversion-of-voltage-drops-of-NTC-sensors-to-temperature/m-p/1863395#M9075</guid>
      <dc:creator>URC</dc:creator>
      <dc:date>2024-05-10T11:01:03Z</dc:date>
    </item>
  </channel>
</rss>