<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックCan FD example for HVBMS S32K344</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Can-FD-example-for-HVBMS-S32K344/m-p/1853417#M9009</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;we are trying to connect the RD-K344BMU with RD33775ACNCEVB using the CAN FD. i am successfully debugging the hvbmu2_775a_read_s32ct on the board but as i understand from freemaster the TDEncoding is using TPL and not the CAN. How can i change the setup of the Model for it to use CAN and not TPL or is there a Project that is already made for CAN.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 24 Apr 2024 11:36:28 GMT</pubDate>
    <dc:creator>yassinechamam</dc:creator>
    <dc:date>2024-04-24T11:36:28Z</dc:date>
    <item>
      <title>Can FD example for HVBMS S32K344</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Can-FD-example-for-HVBMS-S32K344/m-p/1853417#M9009</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;we are trying to connect the RD-K344BMU with RD33775ACNCEVB using the CAN FD. i am successfully debugging the hvbmu2_775a_read_s32ct on the board but as i understand from freemaster the TDEncoding is using TPL and not the CAN. How can i change the setup of the Model for it to use CAN and not TPL or is there a Project that is already made for CAN.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 24 Apr 2024 11:36:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Can-FD-example-for-HVBMS-S32K344/m-p/1853417#M9009</guid>
      <dc:creator>yassinechamam</dc:creator>
      <dc:date>2024-04-24T11:36:28Z</dc:date>
    </item>
  </channel>
</rss>