<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Connecting FreeMaster to S32K344 over CAN in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Connecting-FreeMaster-to-S32K344-over-CAN/m-p/1826078#M8915</link>
    <description>&lt;P&gt;I am trying to connect my&amp;nbsp; #S32K344#&amp;nbsp; to FreeMaster through CAN. While the official NXP docs say that CAN is not supported for the K3 family, I found&lt;A href="https://community.nxp.com/t5/FreeMASTER/FreeMASTER-checksum-error-when-connected-to-S32K3xx-by-CAN/m-p/1658730#M1346" target="_self"&gt;&amp;nbsp;this&lt;/A&gt;&amp;nbsp;post where it is recommended to use the FreeMaster Driver 2.0 which supports CAN for the K1 family because the FlexCAN modules for both families are similar.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I didn't quite understand how this should be done. I am using Simulink for developing my application and the MBDT for the K1xx series has a FreeMaster Config block. In the generated code I can see that the function &lt;EM&gt;freemaster_interface_init()&amp;nbsp;&lt;/EM&gt;and &lt;EM&gt;FMSTR_Init()&amp;nbsp;&lt;/EM&gt;functions are called. So I know I have to somehow use the Driver 2.0, configure the FlexCAN module in my K344's model and call these 2 functions (or equivalent). But I'm not so sure how to do this. Can someone help me with it?&lt;/P&gt;</description>
    <pubDate>Tue, 12 Mar 2024 10:23:07 GMT</pubDate>
    <dc:creator>rishikesh_c</dc:creator>
    <dc:date>2024-03-12T10:23:07Z</dc:date>
    <item>
      <title>Connecting FreeMaster to S32K344 over CAN</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Connecting-FreeMaster-to-S32K344-over-CAN/m-p/1826078#M8915</link>
      <description>&lt;P&gt;I am trying to connect my&amp;nbsp; #S32K344#&amp;nbsp; to FreeMaster through CAN. While the official NXP docs say that CAN is not supported for the K3 family, I found&lt;A href="https://community.nxp.com/t5/FreeMASTER/FreeMASTER-checksum-error-when-connected-to-S32K3xx-by-CAN/m-p/1658730#M1346" target="_self"&gt;&amp;nbsp;this&lt;/A&gt;&amp;nbsp;post where it is recommended to use the FreeMaster Driver 2.0 which supports CAN for the K1 family because the FlexCAN modules for both families are similar.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I didn't quite understand how this should be done. I am using Simulink for developing my application and the MBDT for the K1xx series has a FreeMaster Config block. In the generated code I can see that the function &lt;EM&gt;freemaster_interface_init()&amp;nbsp;&lt;/EM&gt;and &lt;EM&gt;FMSTR_Init()&amp;nbsp;&lt;/EM&gt;functions are called. So I know I have to somehow use the Driver 2.0, configure the FlexCAN module in my K344's model and call these 2 functions (or equivalent). But I'm not so sure how to do this. Can someone help me with it?&lt;/P&gt;</description>
      <pubDate>Tue, 12 Mar 2024 10:23:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Connecting-FreeMaster-to-S32K344-over-CAN/m-p/1826078#M8915</guid>
      <dc:creator>rishikesh_c</dc:creator>
      <dc:date>2024-03-12T10:23:07Z</dc:date>
    </item>
  </channel>
</rss>