<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックRe: MC33771 Evaluation board Input harness (NXP-MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MC33771-Evaluation-board-Input-harness-NXP-MBDT/m-p/1821873#M8899</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/230501"&gt;@Beginner_1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;According to the schematics, you could use the BATT-18 EMULATOR to power the MC33771B SPI as long as the wiring is rerouted for the MC33771B. Please keep in mind the following limitations:&lt;/P&gt;
&lt;P&gt;1. BATT-18EMULATOR does not provide an output to emulate the current, so you should not connect any pins to the SENSE_P and SENSE_N pins of the MC33771B SPI. In this case, you cannot emulate the current input of the MC33771B.&lt;/P&gt;
&lt;P&gt;2. BATT-18EMULATOR can supply outputs between 1.2V and 3V3 and make sure that for the cells&amp;nbsp; 5, 9 and 14, the Jumpers are in the default position, because the BATT_18EMULATOR can also provide negative outputs between -3V3 and -1.2V, which are not valid entries for the MC33771B.&lt;/P&gt;
&lt;P&gt;3. BATT-18EMULATOR is powered up using 5V input only.&lt;/P&gt;
&lt;P&gt;Please take care with the wiring!&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Marius&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 05 Mar 2024 20:44:53 GMT</pubDate>
    <dc:creator>mariuslucianand</dc:creator>
    <dc:date>2024-03-05T20:44:53Z</dc:date>
    <item>
      <title>MC33771 Evaluation board Input harness (NXP-MBDT)</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MC33771-Evaluation-board-Input-harness-NXP-MBDT/m-p/1821849#M8898</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can I use the &lt;A href="https://www.nxp.com/design/design-center/designs/18-cell-battery-pack-emulator-to-supply-mc33774-bcc-evbs:BATT-18EMULATOR" target="_blank" rel="noopener"&gt;18 cell emulator&lt;/A&gt; from NXP as an input to the &lt;A href="https://www.nxp.com/products/power-management/battery-management/battery-cell-controllers/evaluation-board-for-mc33771-with-spi-communication:FRDM33771BSPIEVB" target="_blank" rel="noopener"&gt;FRDM33771BSPIEVB&lt;/A&gt;&amp;nbsp;by changing the wire harness according to the both boards?&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/72088"&gt;@mariuslucianand&lt;/a&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 05 Mar 2024 19:24:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MC33771-Evaluation-board-Input-harness-NXP-MBDT/m-p/1821849#M8898</guid>
      <dc:creator>Beginner_1</dc:creator>
      <dc:date>2024-03-05T19:24:26Z</dc:date>
    </item>
    <item>
      <title>Re: MC33771 Evaluation board Input harness (NXP-MBDT)</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MC33771-Evaluation-board-Input-harness-NXP-MBDT/m-p/1821873#M8899</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/230501"&gt;@Beginner_1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;According to the schematics, you could use the BATT-18 EMULATOR to power the MC33771B SPI as long as the wiring is rerouted for the MC33771B. Please keep in mind the following limitations:&lt;/P&gt;
&lt;P&gt;1. BATT-18EMULATOR does not provide an output to emulate the current, so you should not connect any pins to the SENSE_P and SENSE_N pins of the MC33771B SPI. In this case, you cannot emulate the current input of the MC33771B.&lt;/P&gt;
&lt;P&gt;2. BATT-18EMULATOR can supply outputs between 1.2V and 3V3 and make sure that for the cells&amp;nbsp; 5, 9 and 14, the Jumpers are in the default position, because the BATT_18EMULATOR can also provide negative outputs between -3V3 and -1.2V, which are not valid entries for the MC33771B.&lt;/P&gt;
&lt;P&gt;3. BATT-18EMULATOR is powered up using 5V input only.&lt;/P&gt;
&lt;P&gt;Please take care with the wiring!&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Marius&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 05 Mar 2024 20:44:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MC33771-Evaluation-board-Input-harness-NXP-MBDT/m-p/1821873#M8899</guid>
      <dc:creator>mariuslucianand</dc:creator>
      <dc:date>2024-03-05T20:44:53Z</dc:date>
    </item>
  </channel>
</rss>