<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックRe: MPC5744 MBD :The same pin can be used as input or output</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MPC5744-MBD-The-same-pin-can-be-used-as-input-or-output/m-p/686031#M887</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/fanchang"&gt;fanchang&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;I checked the&amp;nbsp;toolbox capabilities regarding this matter - and i'm sorry to inform you - but such functionality is not supported.&lt;/P&gt;&lt;P&gt;The Simulink Code Generations has 3 main functions where it can place the code: initialize, step and terminate. All that code that configures/initialize a peripheral is placed in the initialize function - that is executed only once at the application start.&amp;nbsp;&lt;/P&gt;&lt;P&gt;In that function we can not have the same pin selected as INPUT and OUTPUT, therefore such scenario not supported.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To be honest i do not know how you could use it without some low level programming to control the state of that pin.&lt;/P&gt;&lt;P&gt;Perhaps you could try to use our standard DSPI block and use the SDPI_Transmit to configure the pins as normal SPI but in the HW to connect the same SIO to both SIN and SOUT from the MPC5744. Then with some logic to read the SOUT only when the&amp;nbsp;&lt;SPAN style="background-color: #ffffff;"&gt;S-35190A is transmitting.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff;"&gt;This use-case looks like a loop back on SPI - so you will receive both the messages you transmit and the messages from the&amp;nbsp;&lt;SPAN&gt;S-35190A. You discard the command message and you end up with the useful information for RTC. That might work.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff;"&gt;&lt;SPAN&gt;You can check this video&amp;nbsp;&lt;A href="https://community.nxp.com/thread/453727"&gt;https://community.nxp.com/thread/453727&lt;/A&gt;&amp;nbsp; to see how you can program the standard SPI.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff;"&gt;&lt;SPAN&gt;Hope this helps you!&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff;"&gt;&lt;SPAN&gt;Daniel&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Jul 2017 12:26:40 GMT</pubDate>
    <dc:creator>Daniel_Popa</dc:creator>
    <dc:date>2017-07-11T12:26:40Z</dc:date>
    <item>
      <title>MPC5744 MBD :The same pin can be used as input or output</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MPC5744-MBD-The-same-pin-can-be-used-as-input-or-output/m-p/686028#M884</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; I set MPC5744's(LQFP144) Pin[14] A5 as the seven pin of &amp;nbsp;SPIO RTC chip (SIO) ，the pin is&amp;nbsp;&lt;SPAN style="color: #333333; background-color: #ffffff; font-size: 18px;"&gt;Nonstandard SPI timing ,so it must&amp;nbsp;&lt;SPAN style="color: #3d3d3d; font-size: 15px;"&gt;be used as input or output,how can I do? &amp;nbsp;The chip is S-35190A (for automotive 3-wire real-time clock. please give a design diagram,thanks!&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Jul 2017 01:52:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MPC5744-MBD-The-same-pin-can-be-used-as-input-or-output/m-p/686028#M884</guid>
      <dc:creator>fanchang</dc:creator>
      <dc:date>2017-07-06T01:52:29Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744 MBD :The same pin can be used as input or output</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MPC5744-MBD-The-same-pin-can-be-used-as-input-or-output/m-p/686029#M885</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/fanchang"&gt;fanchang&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;Can you please clarify what do you mean by a "&lt;STRONG style="color: #ff0000;"&gt;design diagram&lt;/STRONG&gt;" ?&lt;/P&gt;&lt;P&gt;You like to see a Simulink model to implement such functionality or some a HW diagram about how to wire these chips ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Jul 2017 05:16:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MPC5744-MBD-The-same-pin-can-be-used-as-input-or-output/m-p/686029#M885</guid>
      <dc:creator>Daniel_Popa</dc:creator>
      <dc:date>2017-07-06T05:16:31Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744 MBD :The same pin can be used as input or output</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MPC5744-MBD-The-same-pin-can-be-used-as-input-or-output/m-p/686030#M886</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I see.I know the input and output setup related to the time,but I can know how to design“&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/24948iC0F7C05A63AC322C/image-size/large?v=v2&amp;amp;px=999" title="无标题.png" alt="无标题.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;How to set the pin to input and output in no same time by MPC5744 MBD tools?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Jul 2017 05:06:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MPC5744-MBD-The-same-pin-can-be-used-as-input-or-output/m-p/686030#M886</guid>
      <dc:creator>fanchang</dc:creator>
      <dc:date>2017-07-10T05:06:39Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744 MBD :The same pin can be used as input or output</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MPC5744-MBD-The-same-pin-can-be-used-as-input-or-output/m-p/686031#M887</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/fanchang"&gt;fanchang&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;I checked the&amp;nbsp;toolbox capabilities regarding this matter - and i'm sorry to inform you - but such functionality is not supported.&lt;/P&gt;&lt;P&gt;The Simulink Code Generations has 3 main functions where it can place the code: initialize, step and terminate. All that code that configures/initialize a peripheral is placed in the initialize function - that is executed only once at the application start.&amp;nbsp;&lt;/P&gt;&lt;P&gt;In that function we can not have the same pin selected as INPUT and OUTPUT, therefore such scenario not supported.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To be honest i do not know how you could use it without some low level programming to control the state of that pin.&lt;/P&gt;&lt;P&gt;Perhaps you could try to use our standard DSPI block and use the SDPI_Transmit to configure the pins as normal SPI but in the HW to connect the same SIO to both SIN and SOUT from the MPC5744. Then with some logic to read the SOUT only when the&amp;nbsp;&lt;SPAN style="background-color: #ffffff;"&gt;S-35190A is transmitting.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff;"&gt;This use-case looks like a loop back on SPI - so you will receive both the messages you transmit and the messages from the&amp;nbsp;&lt;SPAN&gt;S-35190A. You discard the command message and you end up with the useful information for RTC. That might work.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff;"&gt;&lt;SPAN&gt;You can check this video&amp;nbsp;&lt;A href="https://community.nxp.com/thread/453727"&gt;https://community.nxp.com/thread/453727&lt;/A&gt;&amp;nbsp; to see how you can program the standard SPI.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff;"&gt;&lt;SPAN&gt;Hope this helps you!&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff;"&gt;&lt;SPAN&gt;Daniel&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jul 2017 12:26:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MPC5744-MBD-The-same-pin-can-be-used-as-input-or-output/m-p/686031#M887</guid>
      <dc:creator>Daniel_Popa</dc:creator>
      <dc:date>2017-07-11T12:26:40Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744 MBD :The same pin can be used as input or output</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MPC5744-MBD-The-same-pin-can-be-used-as-input-or-output/m-p/686032#M888</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Hi&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;A _jive_internal="true" data-containerid="-1" data-containertype="-1" data-content-finding="Community" data-objectid="288763" data-objecttype="3" href="https://community.nxp.com/people/fanchang" style="color: #3d9ce7; background-color: #ffffff; border: 0px; padding: 1px 0px 1px calc(12px + 0.35ex);"&gt;fan tianchen&lt;/A&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Can you send to me a MBD Tools for MPC5744?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;My email is &lt;/SPAN&gt;&lt;A class="jive-link-email-small" href="mailto:819364029@qq.com"&gt;819364029@qq.com&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&amp;nbsp;&amp;nbsp;THX;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Linda Xie&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Aug 2018 05:40:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MPC5744-MBD-The-same-pin-can-be-used-as-input-or-output/m-p/686032#M888</guid>
      <dc:creator>xielinda</dc:creator>
      <dc:date>2018-08-24T05:40:11Z</dc:date>
    </item>
  </channel>
</rss>