<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックMPC5744P FCCU Timeout Functionality Issue</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MPC5744P-FCCU-Timeout-Functionality-Issue/m-p/1813747#M8867</link>
    <description>&lt;P&gt;&lt;SPAN&gt;I'm trying to configure some NCFs to have timeout functionality.&lt;BR /&gt;I configured 4 NCFs (7, 8, 10 and 12) with different configurations&amp;nbsp;&lt;BR /&gt;7 &amp;gt;&amp;gt; no reset &amp;amp; timeout enable&lt;BR /&gt;8 &amp;gt;&amp;gt; short reset &amp;amp; timeout enable&lt;BR /&gt;10 &amp;gt;&amp;gt; long reset &amp;amp; timeout enable&lt;BR /&gt;12 &amp;gt;&amp;gt; Eout &amp;amp; timeout enable&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;and in the control tab (changed the timeout to be 65535)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;then i generated code for this configurations and used it with the following sequence:&lt;BR /&gt;1- calling FCCU init function and passing these generated structs to it.&lt;BR /&gt;2- reading the NCF_TO register to ensure that it has 65535 value in it.&lt;BR /&gt;3- injecting a fault for one of the configured NCFs (7, 8, 10, 12).&lt;BR /&gt;4- I notice immediate reset without any waiting for timeout.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;as I understand it shall enter Alarm state and wait there for specific time (the configured timeout) then enters Fault State.&lt;BR /&gt;what I see is that it enters fault state and perform reset immediately.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;any ideas how to solve this?&lt;BR /&gt;also if there is example, that would be very helpful.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 22 Feb 2024 11:10:10 GMT</pubDate>
    <dc:creator>sfathy</dc:creator>
    <dc:date>2024-02-22T11:10:10Z</dc:date>
    <item>
      <title>MPC5744P FCCU Timeout Functionality Issue</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MPC5744P-FCCU-Timeout-Functionality-Issue/m-p/1813747#M8867</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I'm trying to configure some NCFs to have timeout functionality.&lt;BR /&gt;I configured 4 NCFs (7, 8, 10 and 12) with different configurations&amp;nbsp;&lt;BR /&gt;7 &amp;gt;&amp;gt; no reset &amp;amp; timeout enable&lt;BR /&gt;8 &amp;gt;&amp;gt; short reset &amp;amp; timeout enable&lt;BR /&gt;10 &amp;gt;&amp;gt; long reset &amp;amp; timeout enable&lt;BR /&gt;12 &amp;gt;&amp;gt; Eout &amp;amp; timeout enable&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;and in the control tab (changed the timeout to be 65535)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;then i generated code for this configurations and used it with the following sequence:&lt;BR /&gt;1- calling FCCU init function and passing these generated structs to it.&lt;BR /&gt;2- reading the NCF_TO register to ensure that it has 65535 value in it.&lt;BR /&gt;3- injecting a fault for one of the configured NCFs (7, 8, 10, 12).&lt;BR /&gt;4- I notice immediate reset without any waiting for timeout.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;as I understand it shall enter Alarm state and wait there for specific time (the configured timeout) then enters Fault State.&lt;BR /&gt;what I see is that it enters fault state and perform reset immediately.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;any ideas how to solve this?&lt;BR /&gt;also if there is example, that would be very helpful.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 22 Feb 2024 11:10:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MPC5744P-FCCU-Timeout-Functionality-Issue/m-p/1813747#M8867</guid>
      <dc:creator>sfathy</dc:creator>
      <dc:date>2024-02-22T11:10:10Z</dc:date>
    </item>
  </channel>
</rss>