<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Profiler block with referenced models not working in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Profiler-block-with-referenced-models-not-working/m-p/1810637#M8846</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;we are working with the NXP Toolbox and encountered a Problem with the Profiler block, when using it within referenced models:&amp;nbsp;&lt;/P&gt;&lt;P&gt;If building the referenced model as Top-Model, no error occurs. If building the overall model, during the referenced model build the following error occurs ('missing files'):&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Function_Call_Subsystem_private.h:27:29: fatal error: s32k_clock_init.h: No such file or directory #include "s32k_clock_init.h"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Please see also the attachement (example from Profiler with an additional referenced mode).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Is there any workaround or bugfix for this?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Oliver&lt;/P&gt;</description>
    <pubDate>Mon, 19 Feb 2024 07:21:12 GMT</pubDate>
    <dc:creator>Oliver3</dc:creator>
    <dc:date>2024-02-19T07:21:12Z</dc:date>
    <item>
      <title>Profiler block with referenced models not working</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Profiler-block-with-referenced-models-not-working/m-p/1810637#M8846</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;we are working with the NXP Toolbox and encountered a Problem with the Profiler block, when using it within referenced models:&amp;nbsp;&lt;/P&gt;&lt;P&gt;If building the referenced model as Top-Model, no error occurs. If building the overall model, during the referenced model build the following error occurs ('missing files'):&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Function_Call_Subsystem_private.h:27:29: fatal error: s32k_clock_init.h: No such file or directory #include "s32k_clock_init.h"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Please see also the attachement (example from Profiler with an additional referenced mode).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Is there any workaround or bugfix for this?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Oliver&lt;/P&gt;</description>
      <pubDate>Mon, 19 Feb 2024 07:21:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Profiler-block-with-referenced-models-not-working/m-p/1810637#M8846</guid>
      <dc:creator>Oliver3</dc:creator>
      <dc:date>2024-02-19T07:21:12Z</dc:date>
    </item>
  </channel>
</rss>