<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to run motor without using freemaster in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-run-motor-without-using-freemaster/m-p/1802701#M8830</link>
    <description>&lt;LI-SPOILER&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;I am using S32K144 BLDC/PMSM Development Kit. Everything is working fine with S32DS and FreeMASTER.&lt;BR /&gt;what need to be done if I want to run the motor just by deploying the code to the controller using S32DS? So that, I can deploy the code, disconnect the PC and then using Potentiometer I can control the speed of the motor.&lt;BR /&gt;In other words, I want to avoid using FreeMASTER to control the motor.&lt;/LI-SPOILER&gt;</description>
    <pubDate>Tue, 06 Feb 2024 13:38:57 GMT</pubDate>
    <dc:creator>nayan</dc:creator>
    <dc:date>2024-02-06T13:38:57Z</dc:date>
    <item>
      <title>How to run motor without using freemaster</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-run-motor-without-using-freemaster/m-p/1802701#M8830</link>
      <description>&lt;LI-SPOILER&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;I am using S32K144 BLDC/PMSM Development Kit. Everything is working fine with S32DS and FreeMASTER.&lt;BR /&gt;what need to be done if I want to run the motor just by deploying the code to the controller using S32DS? So that, I can deploy the code, disconnect the PC and then using Potentiometer I can control the speed of the motor.&lt;BR /&gt;In other words, I want to avoid using FreeMASTER to control the motor.&lt;/LI-SPOILER&gt;</description>
      <pubDate>Tue, 06 Feb 2024 13:38:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-run-motor-without-using-freemaster/m-p/1802701#M8830</guid>
      <dc:creator>nayan</dc:creator>
      <dc:date>2024-02-06T13:38:57Z</dc:date>
    </item>
    <item>
      <title>Re: How to run motor without using freemaster</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-run-motor-without-using-freemaster/m-p/1811670#M8856</link>
      <description>&lt;P&gt;Hello Nayan.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you for using the&amp;nbsp;&lt;SPAN&gt;S32K144 BLDC/PMSM Development Kit.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Make sure you have the latest packages:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;&lt;A href="https://www.mathworks.com/matlabcentral/fileexchange/64740-nxp-support-package-s32k1xx" target="_blank" rel="nofollow noopener noreferrer"&gt;NXP Support Package for S32K1xx&lt;/A&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;A href="https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=MCTB-EX" target="_blank" rel="nofollow noopener noreferrer"&gt;NXP Model-Based Design Toolbox for S32K1xx version 4.3.0&lt;/A&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;After that you can open the model&amp;nbsp;S32K\src\S32_Examples\s32k14x\mc\PMSM_Demo\PMSM_ClosedLoop:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="stefanvlad_0-1708418446486.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/263951i3406C486BE163E88/image-size/large?v=v2&amp;amp;px=999" role="button" title="stefanvlad_0-1708418446486.png" alt="stefanvlad_0-1708418446486.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;stefanvlad_0-1708418446486.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;In the S32K144 EVB tab, there is the IO Controls block:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="stefanvlad_1-1708418508445.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/263952i82D9D133F0EE04A0/image-size/large?v=v2&amp;amp;px=999" role="button" title="stefanvlad_1-1708418508445.png" alt="stefanvlad_1-1708418508445.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;stefanvlad_1-1708418508445.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;The buttons&amp;nbsp;SW2_SpeedUP and&amp;nbsp;SW3_SpeedDOWN control the start-up and&amp;nbsp;the speed of the motor.&lt;/P&gt;
&lt;P&gt;This is the most reliable method to control the motor without using FreeMaster software.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Stefan V.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 20 Feb 2024 08:51:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-run-motor-without-using-freemaster/m-p/1811670#M8856</guid>
      <dc:creator>stefanvlad</dc:creator>
      <dc:date>2024-02-20T08:51:07Z</dc:date>
    </item>
  </channel>
</rss>