<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to set the parameters in the S12ZVM_FOC_Sensorless. in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-set-the-parameters-in-the-S12ZVM-FOC-Sensorless/m-p/685907#M882</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/fengjiang"&gt;fengjiang&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have a BLDC motor that you want to drive it with this Sensorless model ?&lt;/P&gt;&lt;P&gt;The model was developed for PMSM motors (still possible with BLDC but not optimal).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have hall sensors on your motor? Perhaps you can start with much more simple sensored based application like this one:&amp;nbsp;&lt;A href="https://community.nxp.com/docs/DOC-332664"&gt;Example Model: S12ZVM Trapezoidal Motor Control&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This may give you a chance to get familiar with PWM, GPIO, ADC etc, to validate the basic concepts like driving the PWM and read the currents from ADC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That would be the first things to validate on any application. Without the confidence that you can read the motor phase currents at specific time interval you have no solid base for a sensorless application that requires this information to build the speed estimator model.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You could also try to implement a sort of open loop control - i'm showing such approach in the Motor Control Lecture - in order to spin the motor freely under no-load situation. This would be helpful to have a mechanism to test the speed/position estimation needed for FOC control.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Once you fix all these - then we can discuss all the bells and whistles of the FOC Sensorless control.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please keep us posted with your progress. In know that others will be interested. I know that &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/edenli"&gt;edenli&lt;/A&gt;&amp;nbsp;and &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/dsytj88@126.com"&gt;dsytj88@126.com&lt;/A&gt;&amp;nbsp;are also working on something similar. It will be nice to have some sort of round table on this topic.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regard,&lt;BR /&gt;Daniel&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 27 Jul 2017 19:16:29 GMT</pubDate>
    <dc:creator>Daniel_Popa</dc:creator>
    <dc:date>2017-07-27T19:16:29Z</dc:date>
    <item>
      <title>How to set the parameters in the S12ZVM_FOC_Sensorless.</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-set-the-parameters-in-the-S12ZVM-FOC-Sensorless/m-p/685906#M881</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Dear Daniel&lt;/P&gt;&lt;P&gt;Good Morning!&lt;/P&gt;&lt;P&gt;I can't drive my BLDC with the S12ZVM_FOC_Sensorless.&lt;/P&gt;&lt;P&gt;Could you tell me some ides or attentions about how to set the parameters in the SloopLoopAlgorithm and FastLoopAlgorithm subsystem to drive my BLDC run? Thanks very very much&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Jul 2017 09:45:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-set-the-parameters-in-the-S12ZVM-FOC-Sensorless/m-p/685906#M881</guid>
      <dc:creator>jiangfeng</dc:creator>
      <dc:date>2017-07-27T09:45:08Z</dc:date>
    </item>
    <item>
      <title>Re: How to set the parameters in the S12ZVM_FOC_Sensorless.</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-set-the-parameters-in-the-S12ZVM-FOC-Sensorless/m-p/685907#M882</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/fengjiang"&gt;fengjiang&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have a BLDC motor that you want to drive it with this Sensorless model ?&lt;/P&gt;&lt;P&gt;The model was developed for PMSM motors (still possible with BLDC but not optimal).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have hall sensors on your motor? Perhaps you can start with much more simple sensored based application like this one:&amp;nbsp;&lt;A href="https://community.nxp.com/docs/DOC-332664"&gt;Example Model: S12ZVM Trapezoidal Motor Control&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This may give you a chance to get familiar with PWM, GPIO, ADC etc, to validate the basic concepts like driving the PWM and read the currents from ADC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That would be the first things to validate on any application. Without the confidence that you can read the motor phase currents at specific time interval you have no solid base for a sensorless application that requires this information to build the speed estimator model.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You could also try to implement a sort of open loop control - i'm showing such approach in the Motor Control Lecture - in order to spin the motor freely under no-load situation. This would be helpful to have a mechanism to test the speed/position estimation needed for FOC control.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Once you fix all these - then we can discuss all the bells and whistles of the FOC Sensorless control.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please keep us posted with your progress. In know that others will be interested. I know that &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/edenli"&gt;edenli&lt;/A&gt;&amp;nbsp;and &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/dsytj88@126.com"&gt;dsytj88@126.com&lt;/A&gt;&amp;nbsp;are also working on something similar. It will be nice to have some sort of round table on this topic.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regard,&lt;BR /&gt;Daniel&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Jul 2017 19:16:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-set-the-parameters-in-the-S12ZVM-FOC-Sensorless/m-p/685907#M882</guid>
      <dc:creator>Daniel_Popa</dc:creator>
      <dc:date>2017-07-27T19:16:29Z</dc:date>
    </item>
    <item>
      <title>Re: How to set the parameters in the S12ZVM_FOC_Sensorless.</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-set-the-parameters-in-the-S12ZVM-FOC-Sensorless/m-p/685908#M883</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,my dear friend&lt;/P&gt;&lt;P&gt;The advice you made is very helpful to me ! I will flow what you said above.&lt;/P&gt;&lt;P&gt;Thank you very much for your advice from my heart, Daniel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Jul 2017 01:11:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-set-the-parameters-in-the-S12ZVM-FOC-Sensorless/m-p/685908#M883</guid>
      <dc:creator>jiangfeng</dc:creator>
      <dc:date>2017-07-28T01:11:41Z</dc:date>
    </item>
  </channel>
</rss>