<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックCode from S32 SDK</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Code-from-S32-SDK/m-p/1794934#M8791</link>
    <description>&lt;P&gt;Was wondering if there is a way to import code written with the SDK from S32 into MBDT in simulink. Importing custom code I can do but if the code requires files from SDK how would I go about importing that. For example importing code written with one of the drivers.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 24 Jan 2024 22:44:33 GMT</pubDate>
    <dc:creator>Khang</dc:creator>
    <dc:date>2024-01-24T22:44:33Z</dc:date>
    <item>
      <title>Code from S32 SDK</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Code-from-S32-SDK/m-p/1794934#M8791</link>
      <description>&lt;P&gt;Was wondering if there is a way to import code written with the SDK from S32 into MBDT in simulink. Importing custom code I can do but if the code requires files from SDK how would I go about importing that. For example importing code written with one of the drivers.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 24 Jan 2024 22:44:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Code-from-S32-SDK/m-p/1794934#M8791</guid>
      <dc:creator>Khang</dc:creator>
      <dc:date>2024-01-24T22:44:33Z</dc:date>
    </item>
  </channel>
</rss>