<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic FS32K144 LPIT Channel 2 not working in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/FS32K144-LPIT-Channel-2-not-working/m-p/1762425#M8677</link>
    <description>&lt;P&gt;Hello NXP Community,&lt;/P&gt;&lt;P&gt;While doing a project concerning I2C communication and ADC conversion I have noticed that when setting the LPIT channel to 2 the periodic interrupt did not work. All the other channels (0, 1, 3) work as they are supposed to. Are there some other peripherals which interfere with LPIT ch2 or there has to be an additional initialization for it to work? To program the code I am using NXP MBDT matlab toolbox.&lt;/P&gt;</description>
    <pubDate>Thu, 23 Nov 2023 07:24:43 GMT</pubDate>
    <dc:creator>ErwinR</dc:creator>
    <dc:date>2023-11-23T07:24:43Z</dc:date>
    <item>
      <title>FS32K144 LPIT Channel 2 not working</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/FS32K144-LPIT-Channel-2-not-working/m-p/1762425#M8677</link>
      <description>&lt;P&gt;Hello NXP Community,&lt;/P&gt;&lt;P&gt;While doing a project concerning I2C communication and ADC conversion I have noticed that when setting the LPIT channel to 2 the periodic interrupt did not work. All the other channels (0, 1, 3) work as they are supposed to. Are there some other peripherals which interfere with LPIT ch2 or there has to be an additional initialization for it to work? To program the code I am using NXP MBDT matlab toolbox.&lt;/P&gt;</description>
      <pubDate>Thu, 23 Nov 2023 07:24:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/FS32K144-LPIT-Channel-2-not-working/m-p/1762425#M8677</guid>
      <dc:creator>ErwinR</dc:creator>
      <dc:date>2023-11-23T07:24:43Z</dc:date>
    </item>
  </channel>
</rss>