<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K144 Model Based Design Toolbox CAN Communication problem in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K144-Model-Based-Design-Toolbox-CAN-Communication-problem/m-p/1760116#M8672</link>
    <description>&lt;P&gt;I have solved the problem by resetting the SBC to factory settings again.&lt;/P&gt;</description>
    <pubDate>Mon, 20 Nov 2023 22:50:28 GMT</pubDate>
    <dc:creator>Umutulker</dc:creator>
    <dc:date>2023-11-20T22:50:28Z</dc:date>
    <item>
      <title>S32K144 Model Based Design Toolbox CAN Communication problem</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K144-Model-Based-Design-Toolbox-CAN-Communication-problem/m-p/1753717#M8657</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm experiencing an issue while running CAN examples or my own CAN models on Simulink. I'm attempting to receive a specific message from a real CAN bus. I've tried replicating the logic from the provided examples, but I'm still facing issues. The only time I was able to SEND a message to a CAN Analyzer was with the SBC example model, which configures the LPSPI and SBC. However, configuring the SBC doesn't always work when sending, and I still can't receive any messages even with the SBC configured.&lt;/P&gt;&lt;P&gt;I've verified that the jumper settings are correct, and I'm powering the board with an external 12V DC source while flashing it via micro-USB. I've also attempted to reset the SBC to factory settings without success. I'm connecting CAN HI and CAN LO to the CAN Analyzer or directly to the real CAN Bus.&lt;/P&gt;&lt;P&gt;For reference, I've attached a simple model.&amp;nbsp;&lt;SPAN&gt;When I attempted to use interrupts, I still couldn't observe any changes in the LEDs. It remains in the initial state, which means the message isn't being received.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you for your help.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 07 Nov 2023 21:21:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K144-Model-Based-Design-Toolbox-CAN-Communication-problem/m-p/1753717#M8657</guid>
      <dc:creator>Umutulker</dc:creator>
      <dc:date>2023-11-07T21:21:28Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 Model Based Design Toolbox CAN Communication problem</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K144-Model-Based-Design-Toolbox-CAN-Communication-problem/m-p/1760116#M8672</link>
      <description>&lt;P&gt;I have solved the problem by resetting the SBC to factory settings again.&lt;/P&gt;</description>
      <pubDate>Mon, 20 Nov 2023 22:50:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K144-Model-Based-Design-Toolbox-CAN-Communication-problem/m-p/1760116#M8672</guid>
      <dc:creator>Umutulker</dc:creator>
      <dc:date>2023-11-20T22:50:28Z</dc:date>
    </item>
  </channel>
</rss>