<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックUnable to upload algorithm on S32K344-T172 EVB</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Unable-to-upload-algorithm-on-S32K344-T172-EVB/m-p/1759786#M8671</link>
    <description>&lt;P&gt;I am trying to perform a PIL simulation using NXP S32K344-T172 EVB and Simulink R2022b MBD. I am using NXP Reference Example "s32k3xx_pil_target_s32ct.mdl" and "s32k3xx_pil_harness_s32ct.mdk" for the testing the board. Model is generating the elf file as well as bin file successfully. Also SIL is also performed. But while flashing the algorithm to hardware, I am facing the below attached error.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;The timeout of 10 seconds for receiving data from the rtiostream interface has been exceeded. There might be multiple reasons for this&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;communications failure.&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;You should:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;(a) Check that the target hardware configuration is correct, for example, check that the byte ordering is correct.&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;(b) Confirm that the target application is running on the target hardware.&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;(c) Consider the possibility of application run-time failures (e.g. divide by zero exceptions, incorrect custom code integration, etc.).&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Note (c): To identify possible reasons for the run-time failure, consider using SIL, which supports signal handlers and debugging.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;If you cannot find a solution, consider using the method setTimeoutRecvSecs of rtw.connectivity.RtIOStreamHostCommunicator to increase the&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;timeout value.&lt;/STRONG&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 20 Nov 2023 10:27:26 GMT</pubDate>
    <dc:creator>Nikunj_Patel</dc:creator>
    <dc:date>2023-11-20T10:27:26Z</dc:date>
    <item>
      <title>Unable to upload algorithm on S32K344-T172 EVB</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Unable-to-upload-algorithm-on-S32K344-T172-EVB/m-p/1759786#M8671</link>
      <description>&lt;P&gt;I am trying to perform a PIL simulation using NXP S32K344-T172 EVB and Simulink R2022b MBD. I am using NXP Reference Example "s32k3xx_pil_target_s32ct.mdl" and "s32k3xx_pil_harness_s32ct.mdk" for the testing the board. Model is generating the elf file as well as bin file successfully. Also SIL is also performed. But while flashing the algorithm to hardware, I am facing the below attached error.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;The timeout of 10 seconds for receiving data from the rtiostream interface has been exceeded. There might be multiple reasons for this&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;communications failure.&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;You should:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;(a) Check that the target hardware configuration is correct, for example, check that the byte ordering is correct.&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;(b) Confirm that the target application is running on the target hardware.&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;(c) Consider the possibility of application run-time failures (e.g. divide by zero exceptions, incorrect custom code integration, etc.).&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Note (c): To identify possible reasons for the run-time failure, consider using SIL, which supports signal handlers and debugging.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;If you cannot find a solution, consider using the method setTimeoutRecvSecs of rtw.connectivity.RtIOStreamHostCommunicator to increase the&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;timeout value.&lt;/STRONG&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 20 Nov 2023 10:27:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Unable-to-upload-algorithm-on-S32K344-T172-EVB/m-p/1759786#M8671</guid>
      <dc:creator>Nikunj_Patel</dc:creator>
      <dc:date>2023-11-20T10:27:26Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to upload algorithm on S32K344-T172 EVB</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Unable-to-upload-algorithm-on-S32K344-T172-EVB/m-p/1768303#M8690</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/225618"&gt;@Nikunj_Patel&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Thanks for using MBDT into your projects.&lt;/P&gt;
&lt;P&gt;I've noticed that the S32K3xx toolbox is situated in the typical MATLAB Add-Ons directory, specifically 'AppData\Roaming\MathWorks...'. Given that Windows has a maximum path length of 256 characters, and the P&amp;amp;E Micro programming tool within our toolbox has numerous subfolders, this could result in malfunctions for various tools, as you've experienced. &lt;SPAN&gt;In this instance, the P&amp;amp;E GDB Server issues an error stating that the 'Programming algorithm is not available for this device.'&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;My recommendation is to change your default Add-Ons path to a shorter one to avoid potential problems arising from Windows path limitations.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Please let us know if this helped you.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Victor&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 04 Dec 2023 14:29:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Unable-to-upload-algorithm-on-S32K344-T172-EVB/m-p/1768303#M8690</guid>
      <dc:creator>georgevictor</dc:creator>
      <dc:date>2023-12-04T14:29:06Z</dc:date>
    </item>
  </channel>
</rss>