<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックAutomate storing CAN messages (with multiple signals) using MBDT</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Automate-storing-CAN-messages-with-multiple-signals-using-MBDT/m-p/1757917#M8667</link>
    <description>&lt;P&gt;Hey Guys,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I&amp;nbsp;am trying to create a VCU application that reads/sends multiple CAN messages.&lt;/P&gt;&lt;P&gt;Lets say I have 5 CAN messages that I am trying to Tx/Rx &amp;amp; each CAN message has say 5 CAN signals.&lt;/P&gt;&lt;P&gt;Now I am reading the Rx data &amp;amp; writing it to a Data Store Write block. But I am manually specifying the data store block for each signal. For 5 CAN messages with 5 signals each, it becomes tedious (my application actually has more CAN messages &amp;amp; signals)&lt;/P&gt;&lt;P&gt;I was wondering if there is an easier way of reading the data from CAN Unpack &amp;amp; automate storing them in to a data store block by using the DBC info.&lt;/P&gt;&lt;P&gt;Is there a possibility to do that using MBDT?&lt;/P&gt;&lt;P&gt;Hari&lt;/P&gt;</description>
    <pubDate>Wed, 15 Nov 2023 22:59:36 GMT</pubDate>
    <dc:creator>HariRam_111</dc:creator>
    <dc:date>2023-11-15T22:59:36Z</dc:date>
    <item>
      <title>Automate storing CAN messages (with multiple signals) using MBDT</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Automate-storing-CAN-messages-with-multiple-signals-using-MBDT/m-p/1757917#M8667</link>
      <description>&lt;P&gt;Hey Guys,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I&amp;nbsp;am trying to create a VCU application that reads/sends multiple CAN messages.&lt;/P&gt;&lt;P&gt;Lets say I have 5 CAN messages that I am trying to Tx/Rx &amp;amp; each CAN message has say 5 CAN signals.&lt;/P&gt;&lt;P&gt;Now I am reading the Rx data &amp;amp; writing it to a Data Store Write block. But I am manually specifying the data store block for each signal. For 5 CAN messages with 5 signals each, it becomes tedious (my application actually has more CAN messages &amp;amp; signals)&lt;/P&gt;&lt;P&gt;I was wondering if there is an easier way of reading the data from CAN Unpack &amp;amp; automate storing them in to a data store block by using the DBC info.&lt;/P&gt;&lt;P&gt;Is there a possibility to do that using MBDT?&lt;/P&gt;&lt;P&gt;Hari&lt;/P&gt;</description>
      <pubDate>Wed, 15 Nov 2023 22:59:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Automate-storing-CAN-messages-with-multiple-signals-using-MBDT/m-p/1757917#M8667</guid>
      <dc:creator>HariRam_111</dc:creator>
      <dc:date>2023-11-15T22:59:36Z</dc:date>
    </item>
  </channel>
</rss>