<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックRe: How to use Freemaster with simulink</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-use-Freemaster-with-simulink/m-p/1754135#M8661</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;1. After integrating FreeMASTER into the Simulink application, no new special file is created. The file with the extension &lt;EM&gt;.elf&lt;/EM&gt; is the one that will be used by the FreeMASTER PC application.&lt;BR /&gt;If, by FreeMASTER file, you mean the FreeMASTER project, you can create it by saving the working project in the PC app. This will create a file with the extension &lt;EM&gt;.pmpx&lt;/EM&gt; which stores all the settings and the configured paths.&lt;/P&gt;
&lt;P&gt;2. There are Simulink examples that can be used to understand how FreeMASTER works. In order to add this functionality in your Simulink application you need to add the &lt;EM&gt;FreeMASTER Config&lt;/EM&gt; block into the Simulink canvas next to your model implementation. This block is only available in the &lt;STRONG&gt;&lt;EM&gt;NXP Model-Based Design Toolbox&lt;/EM&gt;&lt;/STRONG&gt;.&lt;/P&gt;
&lt;P&gt;3. If you already have the &lt;EM&gt;.elf&lt;/EM&gt; file you can easily point to it in the FreeMASTER project by going to: &lt;EM&gt;Project -&amp;gt; Options&lt;/EM&gt; -&amp;gt; &lt;EM&gt;MAP Files&lt;/EM&gt; tab -&amp;gt; &lt;U&gt;&lt;EM&gt;Default symbol file&lt;/EM&gt;&lt;/U&gt;. Here you can browse for the file.&lt;/P&gt;
&lt;P&gt;Detailed steps on how to integrate FreeMASTER into your Simulink application can be found in &lt;STRONG&gt;this article:&lt;/STRONG&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Sending-data-via-UART-and-monitoring-signals-with-FreeMASTER/ta-p/1747896" target="_self"&gt;&lt;STRONG&gt;Sending data via UART and monitoring signals with FreeMASTER&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 08 Nov 2023 10:40:17 GMT</pubDate>
    <dc:creator>Adrian_Gherca</dc:creator>
    <dc:date>2023-11-08T10:40:17Z</dc:date>
    <item>
      <title>How to use Freemaster with simulink</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-use-Freemaster-with-simulink/m-p/1753276#M8656</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you help me&lt;/P&gt;&lt;P&gt;1. how I can create freemaster file and how i can link that file to our simulink model to visualize the output&lt;/P&gt;&lt;P&gt;2. if some Freemaster example file is already present can we link that file into our simulink project&lt;/P&gt;&lt;P&gt;3. link means (map elf file into freemaster ) am i right ?&lt;/P&gt;</description>
      <pubDate>Tue, 07 Nov 2023 06:17:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-use-Freemaster-with-simulink/m-p/1753276#M8656</guid>
      <dc:creator>shukla007</dc:creator>
      <dc:date>2023-11-07T06:17:31Z</dc:date>
    </item>
    <item>
      <title>Re: How to use Freemaster with simulink</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-use-Freemaster-with-simulink/m-p/1754135#M8661</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;1. After integrating FreeMASTER into the Simulink application, no new special file is created. The file with the extension &lt;EM&gt;.elf&lt;/EM&gt; is the one that will be used by the FreeMASTER PC application.&lt;BR /&gt;If, by FreeMASTER file, you mean the FreeMASTER project, you can create it by saving the working project in the PC app. This will create a file with the extension &lt;EM&gt;.pmpx&lt;/EM&gt; which stores all the settings and the configured paths.&lt;/P&gt;
&lt;P&gt;2. There are Simulink examples that can be used to understand how FreeMASTER works. In order to add this functionality in your Simulink application you need to add the &lt;EM&gt;FreeMASTER Config&lt;/EM&gt; block into the Simulink canvas next to your model implementation. This block is only available in the &lt;STRONG&gt;&lt;EM&gt;NXP Model-Based Design Toolbox&lt;/EM&gt;&lt;/STRONG&gt;.&lt;/P&gt;
&lt;P&gt;3. If you already have the &lt;EM&gt;.elf&lt;/EM&gt; file you can easily point to it in the FreeMASTER project by going to: &lt;EM&gt;Project -&amp;gt; Options&lt;/EM&gt; -&amp;gt; &lt;EM&gt;MAP Files&lt;/EM&gt; tab -&amp;gt; &lt;U&gt;&lt;EM&gt;Default symbol file&lt;/EM&gt;&lt;/U&gt;. Here you can browse for the file.&lt;/P&gt;
&lt;P&gt;Detailed steps on how to integrate FreeMASTER into your Simulink application can be found in &lt;STRONG&gt;this article:&lt;/STRONG&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Sending-data-via-UART-and-monitoring-signals-with-FreeMASTER/ta-p/1747896" target="_self"&gt;&lt;STRONG&gt;Sending data via UART and monitoring signals with FreeMASTER&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 08 Nov 2023 10:40:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-use-Freemaster-with-simulink/m-p/1754135#M8661</guid>
      <dc:creator>Adrian_Gherca</dc:creator>
      <dc:date>2023-11-08T10:40:17Z</dc:date>
    </item>
  </channel>
</rss>