<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic RDVCU5775EV,  program does not run according to the given period in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/RDVCU5775EV-program-does-not-run-according-to-the-given-period/m-p/1721951#M8514</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using RDVCU5775EVM, Using MBDT with Simulink 2019b.&lt;/P&gt;&lt;P&gt;I found that when I added the application layer algorithm, the program ran slower than the set cycle. For example, I added a StateFlow to the program to control LED light flicker. The sampling time of Stateflow is 0.1, but the blinking frequency of LED light after running is 2.6Hz. In addition, I encapsulated the CAN send module in the atomic subsystem and set the sampling time to be 0.02 (20ms), but the actual collected CAN message cycle is about 50ms.&lt;BR /&gt;Attached is my program, is it because of the complicated calculation of the application layer that affects the running cycle? Or is it caused by another module? Please take a look.&lt;/P&gt;</description>
    <pubDate>Wed, 13 Sep 2023 10:24:25 GMT</pubDate>
    <dc:creator>RegulusCheng</dc:creator>
    <dc:date>2023-09-13T10:24:25Z</dc:date>
    <item>
      <title>RDVCU5775EV,  program does not run according to the given period</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/RDVCU5775EV-program-does-not-run-according-to-the-given-period/m-p/1721951#M8514</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using RDVCU5775EVM, Using MBDT with Simulink 2019b.&lt;/P&gt;&lt;P&gt;I found that when I added the application layer algorithm, the program ran slower than the set cycle. For example, I added a StateFlow to the program to control LED light flicker. The sampling time of Stateflow is 0.1, but the blinking frequency of LED light after running is 2.6Hz. In addition, I encapsulated the CAN send module in the atomic subsystem and set the sampling time to be 0.02 (20ms), but the actual collected CAN message cycle is about 50ms.&lt;BR /&gt;Attached is my program, is it because of the complicated calculation of the application layer that affects the running cycle? Or is it caused by another module? Please take a look.&lt;/P&gt;</description>
      <pubDate>Wed, 13 Sep 2023 10:24:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/RDVCU5775EV-program-does-not-run-according-to-the-given-period/m-p/1721951#M8514</guid>
      <dc:creator>RegulusCheng</dc:creator>
      <dc:date>2023-09-13T10:24:25Z</dc:date>
    </item>
  </channel>
</rss>