<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K144EVB simulink - LIN Communication in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K144EVB-simulink-LIN-Communication/m-p/1717341#M8488</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I would like to understand the generic process of implementing a LIN stack in simulink&lt;/P&gt;&lt;P&gt;for example, I have multiple schedule tables with different cycle times, eg 10ms, 20ms, 50ms, 100ms, 1000ms etc..&lt;/P&gt;&lt;P&gt;How do I define these schedule tables in simulink?&lt;/P&gt;&lt;P&gt;What blocks do i need to use for populating the data for signals in the schedule table?&lt;/P&gt;&lt;P&gt;How do I capture the response signal on the schedule table?&lt;/P&gt;&lt;P&gt;I think I can make use of general task scheduling feature of the MBDT , but how do i define in the appropriate task subsystems which are related to LIN communication?&lt;/P&gt;</description>
    <pubDate>Tue, 05 Sep 2023 16:32:46 GMT</pubDate>
    <dc:creator>deepan1994</dc:creator>
    <dc:date>2023-09-05T16:32:46Z</dc:date>
    <item>
      <title>S32K144EVB simulink - LIN Communication</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K144EVB-simulink-LIN-Communication/m-p/1717341#M8488</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I would like to understand the generic process of implementing a LIN stack in simulink&lt;/P&gt;&lt;P&gt;for example, I have multiple schedule tables with different cycle times, eg 10ms, 20ms, 50ms, 100ms, 1000ms etc..&lt;/P&gt;&lt;P&gt;How do I define these schedule tables in simulink?&lt;/P&gt;&lt;P&gt;What blocks do i need to use for populating the data for signals in the schedule table?&lt;/P&gt;&lt;P&gt;How do I capture the response signal on the schedule table?&lt;/P&gt;&lt;P&gt;I think I can make use of general task scheduling feature of the MBDT , but how do i define in the appropriate task subsystems which are related to LIN communication?&lt;/P&gt;</description>
      <pubDate>Tue, 05 Sep 2023 16:32:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K144EVB-simulink-LIN-Communication/m-p/1717341#M8488</guid>
      <dc:creator>deepan1994</dc:creator>
      <dc:date>2023-09-05T16:32:46Z</dc:date>
    </item>
  </channel>
</rss>