<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックRe: How to use MSDI Analog  input channels with AMUX and eQADC?</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-use-MSDI-Analog-input-channels-with-AMUX-and-eQADC/m-p/1706564#M8414</link>
    <description>&lt;P&gt;I have solved this problem. Before reading first need to send control instructions to the CD1030 chip through SPI communication to specify the specific pin of AMUX output.&lt;BR /&gt;The SPI instruction consists of a 32-bit register, the specific definition of which can be found in the CD1030 datasheet.&lt;BR /&gt;After the pin is specified, the analog value can be obtained by reading the ANA0 channel through the eQADC module, with a reading limit of 3.3V. Inputs higher than 3.3V are read as 3.3V.&lt;/P&gt;</description>
    <pubDate>Thu, 17 Aug 2023 10:38:17 GMT</pubDate>
    <dc:creator>RegulusCheng</dc:creator>
    <dc:date>2023-08-17T10:38:17Z</dc:date>
    <item>
      <title>How to use MSDI Analog  input channels with AMUX and eQADC?</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-use-MSDI-Analog-input-channels-with-AMUX-and-eQADC/m-p/1706189#M8412</link>
      <description>&lt;P&gt;Hi, everyone&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using RDVCU5775EVM with Simulink 2019b&lt;/P&gt;&lt;P&gt;I had some problems using the analog input channel of MSDI.&lt;/P&gt;&lt;P&gt;I had already tested the digital input channels of MSDI, so the CD1030 chip should work normally. But the user manual of CD1030 didn't say much about the AMUX function, so I don't know if I operate correctly.&lt;/P&gt;&lt;P&gt;I noticed that the User Guide of RDVCU5775EVM mentioned that the main chip uses eQADC channel ANA0 to receive the AMUX input of CD1030, so I just configured the eQADC modules to ANA0 and use it as a normal analog input channel, however, the data I get keep at around 7640(DEC), and no matter what voltage I give it, the data don't change.&lt;/P&gt;&lt;P&gt;I wonder if any other configuration should be done with CD1030 MSDI chips. Please help me.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 17 Aug 2023 03:22:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-use-MSDI-Analog-input-channels-with-AMUX-and-eQADC/m-p/1706189#M8412</guid>
      <dc:creator>RegulusCheng</dc:creator>
      <dc:date>2023-08-17T03:22:13Z</dc:date>
    </item>
    <item>
      <title>Re: How to use MSDI Analog  input channels with AMUX and eQADC?</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-use-MSDI-Analog-input-channels-with-AMUX-and-eQADC/m-p/1706190#M8413</link>
      <description>&lt;P&gt;Here is my model, hope it may help.&lt;/P&gt;</description>
      <pubDate>Thu, 17 Aug 2023 03:23:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-use-MSDI-Analog-input-channels-with-AMUX-and-eQADC/m-p/1706190#M8413</guid>
      <dc:creator>RegulusCheng</dc:creator>
      <dc:date>2023-08-17T03:23:43Z</dc:date>
    </item>
    <item>
      <title>Re: How to use MSDI Analog  input channels with AMUX and eQADC?</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-use-MSDI-Analog-input-channels-with-AMUX-and-eQADC/m-p/1706564#M8414</link>
      <description>&lt;P&gt;I have solved this problem. Before reading first need to send control instructions to the CD1030 chip through SPI communication to specify the specific pin of AMUX output.&lt;BR /&gt;The SPI instruction consists of a 32-bit register, the specific definition of which can be found in the CD1030 datasheet.&lt;BR /&gt;After the pin is specified, the analog value can be obtained by reading the ANA0 channel through the eQADC module, with a reading limit of 3.3V. Inputs higher than 3.3V are read as 3.3V.&lt;/P&gt;</description>
      <pubDate>Thu, 17 Aug 2023 10:38:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-use-MSDI-Analog-input-channels-with-AMUX-and-eQADC/m-p/1706564#M8414</guid>
      <dc:creator>RegulusCheng</dc:creator>
      <dc:date>2023-08-17T10:38:17Z</dc:date>
    </item>
  </channel>
</rss>