<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックquestion on MCAT parameters</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/question-on-MCAT-parameters/m-p/1688179#M8358</link>
    <description>&lt;P&gt;good morning,&lt;/P&gt;&lt;P&gt;in the last days i tried to make mcat with different motor using MCAT for RT1050 on SDK version 2.9.1&lt;/P&gt;&lt;P&gt;my doubt concerns the fact that during MCAT procedure the Rs,Ld,Lq values are extrapolated and saved in the appconfig.h file.&lt;/P&gt;&lt;P&gt;When i import this .h file into i.mx Quad motor control App project, the #define associated with Rs,Ld,Lq are not used in the code. How is it possible that they are calculated by the MCAT but then not used by the motor control project?&lt;/P&gt;&lt;P&gt;thanks in advance&lt;/P&gt;</description>
    <pubDate>Fri, 14 Jul 2023 07:04:23 GMT</pubDate>
    <dc:creator>michelet1</dc:creator>
    <dc:date>2023-07-14T07:04:23Z</dc:date>
    <item>
      <title>question on MCAT parameters</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/question-on-MCAT-parameters/m-p/1688179#M8358</link>
      <description>&lt;P&gt;good morning,&lt;/P&gt;&lt;P&gt;in the last days i tried to make mcat with different motor using MCAT for RT1050 on SDK version 2.9.1&lt;/P&gt;&lt;P&gt;my doubt concerns the fact that during MCAT procedure the Rs,Ld,Lq values are extrapolated and saved in the appconfig.h file.&lt;/P&gt;&lt;P&gt;When i import this .h file into i.mx Quad motor control App project, the #define associated with Rs,Ld,Lq are not used in the code. How is it possible that they are calculated by the MCAT but then not used by the motor control project?&lt;/P&gt;&lt;P&gt;thanks in advance&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jul 2023 07:04:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/question-on-MCAT-parameters/m-p/1688179#M8358</guid>
      <dc:creator>michelet1</dc:creator>
      <dc:date>2023-07-14T07:04:23Z</dc:date>
    </item>
  </channel>
</rss>