<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)中的主题 Re: s-function builder</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/s-function-builder/m-p/1684810#M8344</link>
    <description>&lt;P&gt;To build a custom S-function block in Simulink's S-function Builder, you can Prepare the code, Creation an S-function project, Define S-function parameters, Implement S-functions methods, Configure S-function builder, Build the S-function, test and Deploy.&lt;/P&gt;</description>
    <pubDate>Mon, 10 Jul 2023 10:47:11 GMT</pubDate>
    <dc:creator>Martha09</dc:creator>
    <dc:date>2023-07-10T10:47:11Z</dc:date>
    <item>
      <title>s-function builder</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/s-function-builder/m-p/1684806#M8343</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have LED blinking code of s32k148, now I want to build custom block for that I have to port this code in S-function builder block and generate TLC file for same. I want know about procedure for this and also want to know about which files are required for building in s-function builder.&lt;/P&gt;</description>
      <pubDate>Mon, 10 Jul 2023 10:37:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/s-function-builder/m-p/1684806#M8343</guid>
      <dc:creator>saurabhkulkarni123</dc:creator>
      <dc:date>2023-07-10T10:37:58Z</dc:date>
    </item>
    <item>
      <title>Re: s-function builder</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/s-function-builder/m-p/1684810#M8344</link>
      <description>&lt;P&gt;To build a custom S-function block in Simulink's S-function Builder, you can Prepare the code, Creation an S-function project, Define S-function parameters, Implement S-functions methods, Configure S-function builder, Build the S-function, test and Deploy.&lt;/P&gt;</description>
      <pubDate>Mon, 10 Jul 2023 10:47:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/s-function-builder/m-p/1684810#M8344</guid>
      <dc:creator>Martha09</dc:creator>
      <dc:date>2023-07-10T10:47:11Z</dc:date>
    </item>
    <item>
      <title>Re: s-function builder</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/s-function-builder/m-p/1684837#M8345</link>
      <description>I have code where Pin are assign to led, but in s-function builder how can I declare pin.</description>
      <pubDate>Mon, 10 Jul 2023 11:15:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/s-function-builder/m-p/1684837#M8345</guid>
      <dc:creator>saurabhkulkarni123</dc:creator>
      <dc:date>2023-07-10T11:15:27Z</dc:date>
    </item>
  </channel>
</rss>