<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックRe: Cannot program with RappID via CAN</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Cannot-program-with-RappID-via-CAN/m-p/1683066#M8336</link>
    <description>&lt;P&gt;No one had this problem before?&lt;/P&gt;</description>
    <pubDate>Thu, 06 Jul 2023 09:42:18 GMT</pubDate>
    <dc:creator>AsierMaser</dc:creator>
    <dc:date>2023-07-06T09:42:18Z</dc:date>
    <item>
      <title>Cannot program with RappID via CAN</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Cannot-program-with-RappID-via-CAN/m-p/1673382#M8297</link>
      <description>&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;I have some trouble when I try to program my MPC5675K (custom board) via CAN. I am using RAppID BL Tool for that purpose (version 1.6.7.35) and as interface I tried with Vector's CANcaseXL and VN1630 with no luck.&lt;/P&gt;&lt;P&gt;In order to make things easier, I generated a basic program with some peripherals check (comms, IOs, ADCs, etc.). The .mot file was generated in Matlab with Motor Control Toolbox. Here is the configuration of RAppID.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="AsierMaser_0-1687332549017.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/228703i4528A298731D7DEC/image-size/medium?v=v2&amp;amp;px=400" role="button" title="AsierMaser_0-1687332549017.png" alt="AsierMaser_0-1687332549017.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;And this is the message I get when I try to program the micro.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="AsierMaser_1-1687332675837.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/228705i9FCE6BD267033067/image-size/medium?v=v2&amp;amp;px=400" role="button" title="AsierMaser_1-1687332675837.png" alt="AsierMaser_1-1687332675837.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The ABS2, ABS0 and FAB pins are set by hardware as the message says. I also tried with different baud rates with no luck. Is there any detail am I missing?&lt;/P&gt;&lt;P&gt;Any help or ideas are welcome.&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;</description>
      <pubDate>Wed, 21 Jun 2023 07:37:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Cannot-program-with-RappID-via-CAN/m-p/1673382#M8297</guid>
      <dc:creator>AsierMaser</dc:creator>
      <dc:date>2023-06-21T07:37:33Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot program with RappID via CAN</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Cannot-program-with-RappID-via-CAN/m-p/1683066#M8336</link>
      <description>&lt;P&gt;No one had this problem before?&lt;/P&gt;</description>
      <pubDate>Thu, 06 Jul 2023 09:42:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Cannot-program-with-RappID-via-CAN/m-p/1683066#M8336</guid>
      <dc:creator>AsierMaser</dc:creator>
      <dc:date>2023-07-06T09:42:18Z</dc:date>
    </item>
  </channel>
</rss>