<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MBD toolbox for S32K3 does not work in Linux in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBD-toolbox-for-S32K3-does-not-work-in-Linux/m-p/1683029#M8332</link>
    <description>&lt;P&gt;I am using Ubuntu machine for the development&lt;/P&gt;&lt;P&gt;I successfully set up S32 design studio from NXP and was able to flash my&lt;/P&gt;&lt;P&gt;S32K3x4-Q257 board.&lt;/P&gt;&lt;P&gt;Also I was able to install the MBD toolbox, but it fails during the license check.&lt;/P&gt;&lt;P&gt;Since Linux does not have "vol" command I used my Ethernet address to generate license file.&lt;/P&gt;&lt;P&gt;However it always fails license check... I noticed that at NXP_MBDToolbox_S32K3xx/tools/mlt/ folder only has *.exe files that would not work in Linux.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any way to use it with Linux? Toolchain seems to be compatible, only license activation is the problem!&lt;/P&gt;</description>
    <pubDate>Thu, 06 Jul 2023 09:18:50 GMT</pubDate>
    <dc:creator>Nomados</dc:creator>
    <dc:date>2023-07-06T09:18:50Z</dc:date>
    <item>
      <title>MBD toolbox for S32K3 does not work in Linux</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBD-toolbox-for-S32K3-does-not-work-in-Linux/m-p/1683029#M8332</link>
      <description>&lt;P&gt;I am using Ubuntu machine for the development&lt;/P&gt;&lt;P&gt;I successfully set up S32 design studio from NXP and was able to flash my&lt;/P&gt;&lt;P&gt;S32K3x4-Q257 board.&lt;/P&gt;&lt;P&gt;Also I was able to install the MBD toolbox, but it fails during the license check.&lt;/P&gt;&lt;P&gt;Since Linux does not have "vol" command I used my Ethernet address to generate license file.&lt;/P&gt;&lt;P&gt;However it always fails license check... I noticed that at NXP_MBDToolbox_S32K3xx/tools/mlt/ folder only has *.exe files that would not work in Linux.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any way to use it with Linux? Toolchain seems to be compatible, only license activation is the problem!&lt;/P&gt;</description>
      <pubDate>Thu, 06 Jul 2023 09:18:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBD-toolbox-for-S32K3-does-not-work-in-Linux/m-p/1683029#M8332</guid>
      <dc:creator>Nomados</dc:creator>
      <dc:date>2023-07-06T09:18:50Z</dc:date>
    </item>
    <item>
      <title>Re: MBD toolbox for S32K3 does not work in Linux</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBD-toolbox-for-S32K3-does-not-work-in-Linux/m-p/1685072#M8347</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/219928"&gt;@Nomados&lt;/a&gt;,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The Model-Based Design Toolbox is a product developed and tested on Windows only, so, unfortunately, the Linux OS is not supported. For more details about the MBDT system requirements, you can consult the&amp;nbsp;&lt;SPAN&gt;&lt;STRONG&gt;Model_Based_Design_Toolbox_S32K3xx_Series_Quick_Start_Guide&lt;/STRONG&gt; document.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Irina&lt;/P&gt;</description>
      <pubDate>Mon, 10 Jul 2023 16:51:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBD-toolbox-for-S32K3-does-not-work-in-Linux/m-p/1685072#M8347</guid>
      <dc:creator>Irina_Costachescu</dc:creator>
      <dc:date>2023-07-10T16:51:56Z</dc:date>
    </item>
    <item>
      <title>Re: MBD toolbox for S32K3 does not work in Linux</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBD-toolbox-for-S32K3-does-not-work-in-Linux/m-p/1685626#M8351</link>
      <description>&lt;P&gt;Sorry to hear that... Do you have any plans to add support for Linux as well?&lt;/P&gt;</description>
      <pubDate>Tue, 11 Jul 2023 08:45:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBD-toolbox-for-S32K3-does-not-work-in-Linux/m-p/1685626#M8351</guid>
      <dc:creator>Nomados</dc:creator>
      <dc:date>2023-07-11T08:45:45Z</dc:date>
    </item>
  </channel>
</rss>