<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックRe: Code extraction from MATLAB</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Code-extraction-from-MATLAB/m-p/1682975#M8330</link>
    <description>&lt;P&gt;Generate C code in MATLAB: Use MATLAB's code generation feature to generate C code from your MATLAB script or model. Make sure to select the appropriate options for generating standalone C code without any MATLAB dependencies. Create a new project in S32 Design Studio: Open S32 Design Studio for ARM and create a new project by selecting the appropriate microcontroller or device you are targeting. Set up project settings: Configure the project settings, including the toolchain, build configurations, and compiler options, to match your requirements. Add the MATLAB-generated C code files: Copy or import the MATLAB-generated C code files into the S32 Design Studio project. You can either create new source files or add the existing C code files to the project structure. Configure project dependencies: If your MATLAB-generated C code has any external library dependencies, make sure to include the necessary library files and configure the project settings accordingly.&amp;nbsp; &amp;nbsp;&amp;nbsp;&lt;A href="https://www.upsers.app/" target="_self"&gt;UPSers&lt;/A&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 07 Jul 2023 04:01:22 GMT</pubDate>
    <dc:creator>Kieratucker</dc:creator>
    <dc:date>2023-07-07T04:01:22Z</dc:date>
    <item>
      <title>Code extraction from MATLAB</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Code-extraction-from-MATLAB/m-p/1681643#M8327</link>
      <description>&lt;P&gt;I m having Issue importing MATLAB generated C code into S32 design studio for ARM Can you please help me with steps to import this code.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Wed, 05 Jul 2023 05:59:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Code-extraction-from-MATLAB/m-p/1681643#M8327</guid>
      <dc:creator>shiwani</dc:creator>
      <dc:date>2023-07-05T05:59:41Z</dc:date>
    </item>
    <item>
      <title>Re: Code extraction from MATLAB</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Code-extraction-from-MATLAB/m-p/1682975#M8330</link>
      <description>&lt;P&gt;Generate C code in MATLAB: Use MATLAB's code generation feature to generate C code from your MATLAB script or model. Make sure to select the appropriate options for generating standalone C code without any MATLAB dependencies. Create a new project in S32 Design Studio: Open S32 Design Studio for ARM and create a new project by selecting the appropriate microcontroller or device you are targeting. Set up project settings: Configure the project settings, including the toolchain, build configurations, and compiler options, to match your requirements. Add the MATLAB-generated C code files: Copy or import the MATLAB-generated C code files into the S32 Design Studio project. You can either create new source files or add the existing C code files to the project structure. Configure project dependencies: If your MATLAB-generated C code has any external library dependencies, make sure to include the necessary library files and configure the project settings accordingly.&amp;nbsp; &amp;nbsp;&amp;nbsp;&lt;A href="https://www.upsers.app/" target="_self"&gt;UPSers&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 07 Jul 2023 04:01:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Code-extraction-from-MATLAB/m-p/1682975#M8330</guid>
      <dc:creator>Kieratucker</dc:creator>
      <dc:date>2023-07-07T04:01:22Z</dc:date>
    </item>
    <item>
      <title>Re: Code extraction from MATLAB</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Code-extraction-from-MATLAB/m-p/1683039#M8334</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/212909"&gt;@shiwani&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;For achieving your use case, I would propose to you to check the following&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;A href="https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-export-S32K144-MBDT-Generated-Code-to-S32-Design-Studio/m-p/1244814/highlight/true#M5867" target="_self"&gt;link&lt;/A&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;of a thread on our community where this issue is explained.&lt;/P&gt;
&lt;P&gt;In the referenced post, you could find a step by step procedure of how to import your Simulink generated code into the S32DS environment.&lt;/P&gt;
&lt;P&gt;Hope this helps,&lt;/P&gt;
&lt;P&gt;Irina&lt;/P&gt;</description>
      <pubDate>Thu, 06 Jul 2023 09:27:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Code-extraction-from-MATLAB/m-p/1683039#M8334</guid>
      <dc:creator>Irina_Costachescu</dc:creator>
      <dc:date>2023-07-06T09:27:29Z</dc:date>
    </item>
  </channel>
</rss>