<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックRe: NXP Matlab MBDT 2020a support</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/NXP-Matlab-MBDT-2020a-support/m-p/1674454#M8304</link>
    <description>&lt;P&gt;Hi Dragos,&lt;/P&gt;&lt;P&gt;Thanks for the speedy reply. I haven't tried 2021a - I suspect it will work just fine. However I do need to work with Matlab 2020a for this particular project, so switching to a newer version is not an option. If there is a compatibility issue, would an earlier release of the NXP Model-Based Toolbox (like 1.2?) work with Matlab 2020a "natively"? And if so, could I uninstall the current 1.3 toolbox and replace it with this earlier one?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Cosmin&lt;/P&gt;</description>
    <pubDate>Thu, 22 Jun 2023 13:55:07 GMT</pubDate>
    <dc:creator>CosminIon</dc:creator>
    <dc:date>2023-06-22T13:55:07Z</dc:date>
    <item>
      <title>NXP Matlab MBDT 2020a support</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/NXP-Matlab-MBDT-2020a-support/m-p/1674381#M8302</link>
      <description>&lt;P&gt;Hey NXP support,&lt;/P&gt;&lt;P&gt;I'm having some issues getting the MDBT working with Matlab 2020a. Specifically, I'm trying to protect (as an slxp) a simulink model configured with S32K344 as the target hardware (and associated code generation settings). However it keeps trying to call the &lt;EM&gt;readstruct&lt;/EM&gt; function, which was only introduced in later versions on Matlab. Apparently, it's the &lt;EM&gt;epc2map.p&lt;/EM&gt; file where this call takes place. Is there a way to make it compatible with 2020a? I tried the steps described in the start-up guide - installing the Support Package for Arm Cortex-M and running the mbd_s32k3 scripts, but that doesn't seem to help. The same missing &lt;EM&gt;readstruct&lt;/EM&gt; function is reported during the execution of these scripts, too.&lt;/P&gt;&lt;P&gt;I'm using version 1.3 of the toolbox and I'm having no issues protecting models and code-generating on Matlab 2022a (which is officially supported, I suppose).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Many thanks,&lt;/P&gt;&lt;P&gt;Cosmin&lt;/P&gt;</description>
      <pubDate>Thu, 22 Jun 2023 11:28:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/NXP-Matlab-MBDT-2020a-support/m-p/1674381#M8302</guid>
      <dc:creator>CosminIon</dc:creator>
      <dc:date>2023-06-22T11:28:00Z</dc:date>
    </item>
    <item>
      <title>Re: NXP Matlab MBDT 2020a support</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/NXP-Matlab-MBDT-2020a-support/m-p/1674407#M8303</link>
      <description>&lt;P&gt;Hi, &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/218852"&gt;@CosminIon&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Thank you for using MBDT for S32K3xx on your projects.&lt;/P&gt;
&lt;P&gt;Unfortunately, in order to keep up with the most recent MathWorks releases, the NXP S32K3xx 1.3.0 Toolbox is fully compatible with MATLAB versions starting with MATLAB R2021a.&lt;/P&gt;
&lt;P&gt;From what I understand, you tried the R2022a version, and everything works properly. Have you tried using the R2021a version as well? Does it behave correctly?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Dragos&lt;/P&gt;</description>
      <pubDate>Thu, 22 Jun 2023 12:33:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/NXP-Matlab-MBDT-2020a-support/m-p/1674407#M8303</guid>
      <dc:creator>dragostoma</dc:creator>
      <dc:date>2023-06-22T12:33:22Z</dc:date>
    </item>
    <item>
      <title>Re: NXP Matlab MBDT 2020a support</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/NXP-Matlab-MBDT-2020a-support/m-p/1674454#M8304</link>
      <description>&lt;P&gt;Hi Dragos,&lt;/P&gt;&lt;P&gt;Thanks for the speedy reply. I haven't tried 2021a - I suspect it will work just fine. However I do need to work with Matlab 2020a for this particular project, so switching to a newer version is not an option. If there is a compatibility issue, would an earlier release of the NXP Model-Based Toolbox (like 1.2?) work with Matlab 2020a "natively"? And if so, could I uninstall the current 1.3 toolbox and replace it with this earlier one?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Cosmin&lt;/P&gt;</description>
      <pubDate>Thu, 22 Jun 2023 13:55:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/NXP-Matlab-MBDT-2020a-support/m-p/1674454#M8304</guid>
      <dc:creator>CosminIon</dc:creator>
      <dc:date>2023-06-22T13:55:07Z</dc:date>
    </item>
    <item>
      <title>Re: NXP Matlab MBDT 2020a support</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/NXP-Matlab-MBDT-2020a-support/m-p/1674467#M8305</link>
      <description>&lt;P&gt;Quick comment / observation: I believe S32K1 support does extend back to R2020a and older releases but S32K3 doesn't / wouldn't because the MCU wasn't available in 2020. It is a non-trivial effort to propagate support to prior releases. IIRC NXP used R2021a to build he S32K3 support, which was the current SW release at the time of development.&lt;/P&gt;&lt;P&gt;I will note that commonly MathWorks supports the most current 4-6 releases; so even for us R2020a is starting to get old. I would encourage you and your company / project to update to a more current version of MathWorks software, but I also understand sometimes you are locked into a stable / tested / verified MathWorks release; and have to manage using that the best you can.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;-Brian&lt;/P&gt;&lt;P&gt;MathWorks&lt;/P&gt;</description>
      <pubDate>Thu, 22 Jun 2023 14:17:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/NXP-Matlab-MBDT-2020a-support/m-p/1674467#M8305</guid>
      <dc:creator>brianmckay</dc:creator>
      <dc:date>2023-06-22T14:17:00Z</dc:date>
    </item>
    <item>
      <title>Re: NXP Matlab MBDT 2020a support</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/NXP-Matlab-MBDT-2020a-support/m-p/1675971#M8310</link>
      <description>&lt;P&gt;Hey Brian,&lt;/P&gt;&lt;P&gt;Thanks for the feedback - that's good to know. We're normally running on newer versions of Matlab, it's just this project involving external partners which I was struggling with. Interestingly, what seems to have solved my issue is switching to version 1.2 of the S32K3xx toolbox - all works as expected now, not sure if intended or just a happy coincidence...&lt;/P&gt;&lt;P&gt;Cosmin&lt;/P&gt;</description>
      <pubDate>Mon, 26 Jun 2023 10:53:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/NXP-Matlab-MBDT-2020a-support/m-p/1675971#M8310</guid>
      <dc:creator>CosminIon</dc:creator>
      <dc:date>2023-06-26T10:53:36Z</dc:date>
    </item>
  </channel>
</rss>