<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RDVCU5775EVM borad with Simulink 2023a, problems with CAN communication interfaces in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/RDVCU5775EVM-borad-with-Simulink-2023a-problems-with-CAN/m-p/1668078#M8276</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;just for the board connection...&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;The board user guide gives info which MCU pin is connected to available CAN transceivers, see chapters&lt;/SPAN&gt;&lt;BR clear="none" /&gt;&lt;SPAN&gt;2.3.1.5 Communication interface&lt;/SPAN&gt;&lt;BR clear="none" /&gt;&lt;SPAN&gt;2.3.6 CAN transceiver&lt;BR /&gt;&lt;/SPAN&gt;Finally refer to Table 3. Board interface connector details&lt;BR /&gt;&lt;A style="font-family: inherit; background-color: #ffffff;" href="https://www.nxp.com/webapp/Download?colCode=RDVCU5775EVM_UG" target="_blank" rel="noopener"&gt;https://www.nxp.com/webapp/Download?colCode=RDVCU5775EVM_UG&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Pins functions are listed in&amp;nbsp;MPC5775B_MPC5775E_System_IO_Definition.xlsx attached to the device Reference Manual, however "PTE5" notation is not used here.&lt;/SPAN&gt;&lt;BR clear="none" /&gt;&lt;SPAN&gt;You can refer to attached one generated from board's SDK demo project.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;So from above one, no transceiver is connected&amp;nbsp;to PTE5/PTE1 you selected&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR, Petr&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 13 Jun 2023 07:36:43 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2023-06-13T07:36:43Z</dc:date>
    <item>
      <title>RDVCU5775EVM borad with Simulink 2023a, problems with CAN communication interfaces</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/RDVCU5775EVM-borad-with-Simulink-2023a-problems-with-CAN/m-p/1666748#M8275</link>
      <description>&lt;P&gt;Hi, I am trying to develop an RPC with the board of RDVCU5775EVM, and I have some problems when testing the MBDT. am using Simulink 2023a, MBDT3.2.0 20200414, Here are my problems:&lt;/P&gt;&lt;P&gt;1. When setting MBD MPC574x Config_Information to MPC5775B, the FlexCAN function has an error when built and downloaded to the board.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="RegulusCheng_3-1686296537045.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/226972iAA384470F0FB1F10/image-size/medium?v=v2&amp;amp;px=400" alt="RegulusCheng_3-1686296537045.png" title="RegulusCheng_3-1686296537045.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;It seems that the parameters of the FlexCAN module are not recognized.&lt;/P&gt;&lt;P&gt;2. After changing the setting MBD MPC574x Config_Information to MPC5777C, the model can be built and downloaded, but has some problems, too.&lt;/P&gt;&lt;P&gt;The Messages transformed by the FlexCAN module can be received correctly, but Messages generated by a CANTranser can not be received by the RDVCU5775EVM, because the FCAN_Isr trigger seems not to act as well.&lt;/P&gt;&lt;P&gt;The MCAN module can not Trans nor receive, I can't receive the message transformed by MCAN0 nor Trans a message to the board.&amp;nbsp; there are no error frames when I send a message to the MCAN0 channel, but when I link the length parameter of MCAN_Isr(RX completed) to the second byte of FCAN data, the message I received remains zero.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="RegulusCheng_4-1686296584164.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/226973i634033EB5F9F4D67/image-size/medium?v=v2&amp;amp;px=400" alt="RegulusCheng_4-1686296584164.png" title="RegulusCheng_4-1686296584164.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I wonder which Pin should I choose when using MCAN0, I don't know if I choose the correct one. And where can I get the mapping of MPC5775 Pins and RDVCU5775EVM J8?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="RegulusCheng_5-1686296611891.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/226974i47577518AB902C6B/image-size/medium?v=v2&amp;amp;px=400" alt="RegulusCheng_5-1686296611891.png" title="RegulusCheng_5-1686296611891.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;does anyone have the same problem? Or any suggestions? glad to see the reply.&lt;/P&gt;</description>
      <pubDate>Fri, 09 Jun 2023 07:49:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/RDVCU5775EVM-borad-with-Simulink-2023a-problems-with-CAN/m-p/1666748#M8275</guid>
      <dc:creator>RegulusCheng</dc:creator>
      <dc:date>2023-06-09T07:49:40Z</dc:date>
    </item>
    <item>
      <title>Re: RDVCU5775EVM borad with Simulink 2023a, problems with CAN communication interfaces</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/RDVCU5775EVM-borad-with-Simulink-2023a-problems-with-CAN/m-p/1668078#M8276</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;just for the board connection...&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;The board user guide gives info which MCU pin is connected to available CAN transceivers, see chapters&lt;/SPAN&gt;&lt;BR clear="none" /&gt;&lt;SPAN&gt;2.3.1.5 Communication interface&lt;/SPAN&gt;&lt;BR clear="none" /&gt;&lt;SPAN&gt;2.3.6 CAN transceiver&lt;BR /&gt;&lt;/SPAN&gt;Finally refer to Table 3. Board interface connector details&lt;BR /&gt;&lt;A style="font-family: inherit; background-color: #ffffff;" href="https://www.nxp.com/webapp/Download?colCode=RDVCU5775EVM_UG" target="_blank" rel="noopener"&gt;https://www.nxp.com/webapp/Download?colCode=RDVCU5775EVM_UG&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Pins functions are listed in&amp;nbsp;MPC5775B_MPC5775E_System_IO_Definition.xlsx attached to the device Reference Manual, however "PTE5" notation is not used here.&lt;/SPAN&gt;&lt;BR clear="none" /&gt;&lt;SPAN&gt;You can refer to attached one generated from board's SDK demo project.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;So from above one, no transceiver is connected&amp;nbsp;to PTE5/PTE1 you selected&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR, Petr&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 13 Jun 2023 07:36:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/RDVCU5775EVM-borad-with-Simulink-2023a-problems-with-CAN/m-p/1668078#M8276</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2023-06-13T07:36:43Z</dc:date>
    </item>
  </channel>
</rss>