<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How do I use MC33771C with the S32K3XX toolbox? Also, MC3366X loopback help. in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-do-I-use-MC33771C-with-the-S32K3XX-toolbox-Also-MC3366X/m-p/1645662#M8208</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am trying to select components that I can use with the S32K3 toolbox. I was wanting to use teh MC33771C but it looks like the Simulink toolbox only supports the MC33775 which I can't get and the MC33772C which is only for 6 cells. How do I use the toobox with the 14 cell variation? This IC is in the S32K1 toolbox, can I use this toolbox's blocks in my S32K3 based code?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, for loopback would I need 2x MC33664 devices? Is this device usable in the S32K3 toolbox as well? Lastly what does the loopback of TPL benefit?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
    <pubDate>Fri, 05 May 2023 16:38:50 GMT</pubDate>
    <dc:creator>Poley</dc:creator>
    <dc:date>2023-05-05T16:38:50Z</dc:date>
    <item>
      <title>How do I use MC33771C with the S32K3XX toolbox? Also, MC3366X loopback help.</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-do-I-use-MC33771C-with-the-S32K3XX-toolbox-Also-MC3366X/m-p/1645662#M8208</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am trying to select components that I can use with the S32K3 toolbox. I was wanting to use teh MC33771C but it looks like the Simulink toolbox only supports the MC33775 which I can't get and the MC33772C which is only for 6 cells. How do I use the toobox with the 14 cell variation? This IC is in the S32K1 toolbox, can I use this toolbox's blocks in my S32K3 based code?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, for loopback would I need 2x MC33664 devices? Is this device usable in the S32K3 toolbox as well? Lastly what does the loopback of TPL benefit?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Fri, 05 May 2023 16:38:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-do-I-use-MC33771C-with-the-S32K3XX-toolbox-Also-MC3366X/m-p/1645662#M8208</guid>
      <dc:creator>Poley</dc:creator>
      <dc:date>2023-05-05T16:38:50Z</dc:date>
    </item>
    <item>
      <title>Re: How do I use MC33771C with the S32K3XX toolbox? Also, MC3366X loopback help.</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-do-I-use-MC33771C-with-the-S32K3XX-toolbox-Also-MC3366X/m-p/1648074#M8213</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/72088"&gt;@mariuslucianand&lt;/a&gt;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/24319"&gt;@paulvlase&lt;/a&gt;&amp;nbsp; - Do you have any suggestions? Thank you!&lt;/P&gt;</description>
      <pubDate>Wed, 10 May 2023 16:49:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-do-I-use-MC33771C-with-the-S32K3XX-toolbox-Also-MC3366X/m-p/1648074#M8213</guid>
      <dc:creator>Poley</dc:creator>
      <dc:date>2023-05-10T16:49:03Z</dc:date>
    </item>
    <item>
      <title>Re: How do I use MC33771C with the S32K3XX toolbox? Also, MC3366X loopback help.</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-do-I-use-MC33771C-with-the-S32K3XX-toolbox-Also-MC3366X/m-p/1648175#M8214</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/183842"&gt;@Poley&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;MBDT for S32K3 works in a different way than the MBDT for S32K1 works. The MBDT for S32K3 is based on the Real-Time Drivers and generates the configuration codes for the MCU using external configuration tools and not using the configuration blocks as the S32K1. This is why, on each of the MBDT blocks for the K3, you will find the Configure and the Refresh Button. Pressing the Configure button, opens the external configuration tools, like the EBTresos or S32 Configuration tools, allowing to assign pins and configure peripherals while pressing the Refresh button reads the settings from the configuration tools and updates the options inside dropdowns of the blocks.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="mariuslucianand_0-1683755629912.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/222619i059BC0232743CB60/image-size/medium?v=v2&amp;amp;px=400" role="button" title="mariuslucianand_0-1683755629912.png" alt="mariuslucianand_0-1683755629912.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;From the options on top, and also my explanations, you could see that there is a strong bond between the MBDT and the RTD. Coming back to your question, the MBDT only supports the MC33775A for battery cell controllers and the MC33772C (which is the HVBMS this is used only as a current measurement for the Battery Junction Box). In other words, the BMS drivers support only MC33775A and the MC33772C therefore the MC33771C is not supported, MC33775A being its replacement. Unfortunately, the Simulink blocks could not be used across Toolboxes, so the blocks from the MBDT for S32K1xx could not be used for the MBDT for S32K3xx.&lt;/P&gt;
&lt;P&gt;For the loopback, on the HVBMS there is used the newer MC33665, is the replacement for the MC33664, and this has 4 ports for the TPL, therefore you don't need to use 2xMC33664 for loopback, 1xMC33665 will be just fine to address also the loopback.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Marius&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 10 May 2023 22:03:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-do-I-use-MC33771C-with-the-S32K3XX-toolbox-Also-MC3366X/m-p/1648175#M8214</guid>
      <dc:creator>mariuslucianand</dc:creator>
      <dc:date>2023-05-10T22:03:54Z</dc:date>
    </item>
    <item>
      <title>Re: How do I use MC33771C with the S32K3XX toolbox? Also, MC3366X loopback help.</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-do-I-use-MC33771C-with-the-S32K3XX-toolbox-Also-MC3366X/m-p/1648176#M8215</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/72088"&gt;@mariuslucianand&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Yep that all makes complete sense! One other question on the MC33664 loopback if possible. How do I implement a loopback in the toolbox for the S32K1? Is there an example of this? I can only find how to use 1 MC33664.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am making one more S32K1 board before moving to S32K3 and I need loopback functionality with the MC33771C.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;thanks!&lt;/P&gt;</description>
      <pubDate>Wed, 10 May 2023 22:11:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-do-I-use-MC33771C-with-the-S32K3XX-toolbox-Also-MC3366X/m-p/1648176#M8215</guid>
      <dc:creator>Poley</dc:creator>
      <dc:date>2023-05-10T22:11:27Z</dc:date>
    </item>
  </channel>
</rss>