<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックs12zvm MBD</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/s12zvm-MBD/m-p/1625343#M8117</link>
    <description>&lt;P&gt;We got some issues when we configuration the MBD ,May you help to guide us fixed it?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Problems with automatic code generation using &lt;STRONG&gt;S12ZVMX&lt;/STRONG&gt; MBD toolbox&lt;BR /&gt;1 System clock cannot be configured to 16MHz&lt;BR /&gt;2 .c contains wrong header file, even if it is not generated (not supported for compact style code)&lt;BR /&gt;3 Model compilation cannot find predefined files&lt;BR /&gt;4 LIN interrupt interface is not compatible&lt;BR /&gt;5 LIN lacks set idle, wakeup function interface&lt;BR /&gt;6 LIN interface data type is uint16, and the base software in uint8 does not match the problem&lt;BR /&gt;7 LIN initializes the register &amp;nbsp;miss the interrupt &amp;nbsp;registers &amp;nbsp;configuration&lt;/P&gt;&lt;P&gt;8 no need register configuration case, how to read the value of the MCU register&lt;BR /&gt;9 Timer configuration, no channel_0, cannot configure the system clock&lt;BR /&gt;10 ADC system default clock is 50MHz, cannot be modified&lt;BR /&gt;11 ADC does not detect the conversion completion flag without using interrupts&lt;BR /&gt;12 How to use the others defined MCU registers&lt;BR /&gt;13 CPU module only contains the basic clock configuration, no peripheral initialization, and the basic software compatibility is difficult&lt;/P&gt;</description>
    <pubDate>Thu, 30 Mar 2023 13:27:54 GMT</pubDate>
    <dc:creator>SpencerYu</dc:creator>
    <dc:date>2023-03-30T13:27:54Z</dc:date>
    <item>
      <title>s12zvm MBD</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/s12zvm-MBD/m-p/1625343#M8117</link>
      <description>&lt;P&gt;We got some issues when we configuration the MBD ,May you help to guide us fixed it?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Problems with automatic code generation using &lt;STRONG&gt;S12ZVMX&lt;/STRONG&gt; MBD toolbox&lt;BR /&gt;1 System clock cannot be configured to 16MHz&lt;BR /&gt;2 .c contains wrong header file, even if it is not generated (not supported for compact style code)&lt;BR /&gt;3 Model compilation cannot find predefined files&lt;BR /&gt;4 LIN interrupt interface is not compatible&lt;BR /&gt;5 LIN lacks set idle, wakeup function interface&lt;BR /&gt;6 LIN interface data type is uint16, and the base software in uint8 does not match the problem&lt;BR /&gt;7 LIN initializes the register &amp;nbsp;miss the interrupt &amp;nbsp;registers &amp;nbsp;configuration&lt;/P&gt;&lt;P&gt;8 no need register configuration case, how to read the value of the MCU register&lt;BR /&gt;9 Timer configuration, no channel_0, cannot configure the system clock&lt;BR /&gt;10 ADC system default clock is 50MHz, cannot be modified&lt;BR /&gt;11 ADC does not detect the conversion completion flag without using interrupts&lt;BR /&gt;12 How to use the others defined MCU registers&lt;BR /&gt;13 CPU module only contains the basic clock configuration, no peripheral initialization, and the basic software compatibility is difficult&lt;/P&gt;</description>
      <pubDate>Thu, 30 Mar 2023 13:27:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/s12zvm-MBD/m-p/1625343#M8117</guid>
      <dc:creator>SpencerYu</dc:creator>
      <dc:date>2023-03-30T13:27:54Z</dc:date>
    </item>
  </channel>
</rss>