<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)中的主题 FCAN blocks source code for mexw</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/FCAN-blocks-source-code-for-mexw/m-p/1584671#M7990</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I’m developing a model for an MPC5744P using the MBDT. In my model I use the FCAN Send &amp;amp; Receive blocks for CAN communications. But because of some requirements, I had to modify the TLC files of these blocks. Originally, I simply modified the files in my installation of the MBDT. But now I want to share it with some colleagues, so I would rather have the modified TLC within the Simulink project, without changing the original installation of the MBDT.&lt;/P&gt;&lt;P&gt;I would you do this? I have tried a couple of things:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Put the TLC in my Simulink project, hoping Simulink would pick it before picking the file in the original installation of the MBDT. It does not.&lt;/LI&gt;&lt;LI&gt;Try to create new blocks of the FCAN Send and Receive blocks, but have them call the modified TLCs. The TLCs should have another name. The problem is that I need to change the name of the MEXW files as well. If I do this, an error pops up because the name defined within the precompiled MEXW does not match the name of the MEXW. Does anybody have the original C files so that I can adapt them?&lt;/LI&gt;&lt;/OL&gt;</description>
    <pubDate>Wed, 18 Jan 2023 13:59:03 GMT</pubDate>
    <dc:creator>mikel1</dc:creator>
    <dc:date>2023-01-18T13:59:03Z</dc:date>
    <item>
      <title>FCAN blocks source code for mexw</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/FCAN-blocks-source-code-for-mexw/m-p/1584671#M7990</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I’m developing a model for an MPC5744P using the MBDT. In my model I use the FCAN Send &amp;amp; Receive blocks for CAN communications. But because of some requirements, I had to modify the TLC files of these blocks. Originally, I simply modified the files in my installation of the MBDT. But now I want to share it with some colleagues, so I would rather have the modified TLC within the Simulink project, without changing the original installation of the MBDT.&lt;/P&gt;&lt;P&gt;I would you do this? I have tried a couple of things:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Put the TLC in my Simulink project, hoping Simulink would pick it before picking the file in the original installation of the MBDT. It does not.&lt;/LI&gt;&lt;LI&gt;Try to create new blocks of the FCAN Send and Receive blocks, but have them call the modified TLCs. The TLCs should have another name. The problem is that I need to change the name of the MEXW files as well. If I do this, an error pops up because the name defined within the precompiled MEXW does not match the name of the MEXW. Does anybody have the original C files so that I can adapt them?&lt;/LI&gt;&lt;/OL&gt;</description>
      <pubDate>Wed, 18 Jan 2023 13:59:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/FCAN-blocks-source-code-for-mexw/m-p/1584671#M7990</guid>
      <dc:creator>mikel1</dc:creator>
      <dc:date>2023-01-18T13:59:03Z</dc:date>
    </item>
  </channel>
</rss>