<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: EPROM access in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/EPROM-access/m-p/1583815#M7988</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/202837"&gt;@saurabhkulkarni123&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can check out the Flash EEPROM example from the toolbox. That example shows you how you can read and write data from/in the EEPROM memory, using Flash blocks. To visualize the data from EEPROM, FreeMASTER is used. You can find that example made for S32K144 in the following path: &lt;STRONG&gt;{toolbox_path}\src\S32_Examples\s32k14x\flash\flash_eeprom_s32k14x.mdl&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Stefan.&lt;/P&gt;</description>
    <pubDate>Tue, 17 Jan 2023 08:46:11 GMT</pubDate>
    <dc:creator>stefancinipeanu</dc:creator>
    <dc:date>2023-01-17T08:46:11Z</dc:date>
    <item>
      <title>EPROM access</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/EPROM-access/m-p/1582879#M7986</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I want to store data in EEPROM of S32K144 NXP in MBDT, How I can store it, and how to check whether data are stored or not? Or is there any other way to store data in MBDT?&lt;/P&gt;</description>
      <pubDate>Mon, 16 Jan 2023 04:49:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/EPROM-access/m-p/1582879#M7986</guid>
      <dc:creator>saurabhkulkarni123</dc:creator>
      <dc:date>2023-01-16T04:49:38Z</dc:date>
    </item>
    <item>
      <title>Re: EPROM access</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/EPROM-access/m-p/1583815#M7988</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/202837"&gt;@saurabhkulkarni123&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can check out the Flash EEPROM example from the toolbox. That example shows you how you can read and write data from/in the EEPROM memory, using Flash blocks. To visualize the data from EEPROM, FreeMASTER is used. You can find that example made for S32K144 in the following path: &lt;STRONG&gt;{toolbox_path}\src\S32_Examples\s32k14x\flash\flash_eeprom_s32k14x.mdl&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Stefan.&lt;/P&gt;</description>
      <pubDate>Tue, 17 Jan 2023 08:46:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/EPROM-access/m-p/1583815#M7988</guid>
      <dc:creator>stefancinipeanu</dc:creator>
      <dc:date>2023-01-17T08:46:11Z</dc:date>
    </item>
    <item>
      <title>Re: EPROM access</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/EPROM-access/m-p/1589702#M8011</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;very Informative post for storing your values you can do -&lt;/P&gt;&lt;P&gt;Saving a value to EEPROM&lt;BR /&gt;Don't write multiple values on the same address, otherwise you will lose the previously written number (unless that's what you want to do)&lt;BR /&gt;A memory location can only store one byte of data.&lt;BR /&gt;Don't write a value to the EEPROM inside an infinite loop without any delay or check for user input.&lt;/P&gt;&lt;P&gt;Hope so it will helps you&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://apps.apple.com/vn/app/dinar-chronics/id1642043789" target="_self"&gt;dinar chronicles&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 31 Jan 2023 04:27:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/EPROM-access/m-p/1589702#M8011</guid>
      <dc:creator>bixby6245</dc:creator>
      <dc:date>2023-01-31T04:27:07Z</dc:date>
    </item>
  </channel>
</rss>