<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックMBD model - RAppID bootloader - flash by CAN</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBD-model-RAppID-bootloader-flash-by-CAN/m-p/1576099#M7959</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;I'm using the RAppID tool in flashing, by CAN, the .mot file which is generated by MPC 5744P toolbox simulink model. Then, I updated the linker script according to the requirements of the Bootloader. However, sometimes the application started successfully and sometimes the application didn't start after flashing the .mot file.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Why does that behavior happen?&lt;/P&gt;</description>
    <pubDate>Mon, 02 Jan 2023 12:57:34 GMT</pubDate>
    <dc:creator>abdelrhman</dc:creator>
    <dc:date>2023-01-02T12:57:34Z</dc:date>
    <item>
      <title>MBD model - RAppID bootloader - flash by CAN</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBD-model-RAppID-bootloader-flash-by-CAN/m-p/1576099#M7959</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;I'm using the RAppID tool in flashing, by CAN, the .mot file which is generated by MPC 5744P toolbox simulink model. Then, I updated the linker script according to the requirements of the Bootloader. However, sometimes the application started successfully and sometimes the application didn't start after flashing the .mot file.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Why does that behavior happen?&lt;/P&gt;</description>
      <pubDate>Mon, 02 Jan 2023 12:57:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBD-model-RAppID-bootloader-flash-by-CAN/m-p/1576099#M7959</guid>
      <dc:creator>abdelrhman</dc:creator>
      <dc:date>2023-01-02T12:57:34Z</dc:date>
    </item>
  </channel>
</rss>