<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックRe: How to configure ADC using MIMXRT1170-EVK?</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-configure-ADC-using-MIMXRT1170-EVK/m-p/1575998#M7958</link>
    <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;I am just sharing here&amp;nbsp;The MCUXpresso Config Tools are fully integrated into the MCUXpresso IDE, and also available as a standalone download for use with other supported IDEs, including Arm Keil, IAR EWARM and others. If using the MCUXpresso IDE, no additional download of Config Tools is required.&lt;/P&gt;&lt;P&gt;Hope so this information will help in resolving your&amp;nbsp; issue .&lt;/P&gt;&lt;H3&gt;&amp;nbsp;&lt;/H3&gt;</description>
    <pubDate>Mon, 02 Jan 2023 08:56:22 GMT</pubDate>
    <dc:creator>winter0147</dc:creator>
    <dc:date>2023-01-02T08:56:22Z</dc:date>
    <item>
      <title>How to configure ADC using MIMXRT1170-EVK?</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-configure-ADC-using-MIMXRT1170-EVK/m-p/1562705#M7898</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to set up the ADC without any interrupts but when I try to run it, it fails. I don't know if the configuration in MCUxpresso config tools is adecuated or if something is missing.&lt;/P&gt;&lt;P&gt;I attached the model which I am trying to compile.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Thu, 01 Dec 2022 09:24:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-configure-ADC-using-MIMXRT1170-EVK/m-p/1562705#M7898</guid>
      <dc:creator>esantana</dc:creator>
      <dc:date>2022-12-01T09:24:49Z</dc:date>
    </item>
    <item>
      <title>Re: How to configure ADC using MIMXRT1170-EVK?</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-configure-ADC-using-MIMXRT1170-EVK/m-p/1563832#M7905</link>
      <description>&lt;P&gt;The MIMXRT1170 SoC is configured to use the 24 MHz external oscillator on the board with the on-chip PLL to generate a 1 GHz core clock.&lt;/P&gt;</description>
      <pubDate>Sat, 03 Dec 2022 06:20:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-configure-ADC-using-MIMXRT1170-EVK/m-p/1563832#M7905</guid>
      <dc:creator>Tyler691</dc:creator>
      <dc:date>2022-12-03T06:20:38Z</dc:date>
    </item>
    <item>
      <title>Re: How to configure ADC using MIMXRT1170-EVK?</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-configure-ADC-using-MIMXRT1170-EVK/m-p/1575998#M7958</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;I am just sharing here&amp;nbsp;The MCUXpresso Config Tools are fully integrated into the MCUXpresso IDE, and also available as a standalone download for use with other supported IDEs, including Arm Keil, IAR EWARM and others. If using the MCUXpresso IDE, no additional download of Config Tools is required.&lt;/P&gt;&lt;P&gt;Hope so this information will help in resolving your&amp;nbsp; issue .&lt;/P&gt;&lt;H3&gt;&amp;nbsp;&lt;/H3&gt;</description>
      <pubDate>Mon, 02 Jan 2023 08:56:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-configure-ADC-using-MIMXRT1170-EVK/m-p/1575998#M7958</guid>
      <dc:creator>winter0147</dc:creator>
      <dc:date>2023-01-02T08:56:22Z</dc:date>
    </item>
    <item>
      <title>Re: How to configure ADC using MIMXRT1170-EVK?</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-configure-ADC-using-MIMXRT1170-EVK/m-p/1583798#M7987</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/207487"&gt;@esantana&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;We have tested the ADC peripheral and we are not aware of any limitations. Did you try to run the ADC example on polling from MBDT IMXRT toolbox? What kind of error did you get when trying to build the application?&lt;/P&gt;
&lt;P&gt;Usually, to use ADC in polling mode you just have to disable ADC interrupt from configuration file attached to the model, as depicted below:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="stefancinipeanu_0-1673943997728.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/207619i57BD6AD82D920CCD/image-size/medium?v=v2&amp;amp;px=400" role="button" title="stefancinipeanu_0-1673943997728.png" alt="stefancinipeanu_0-1673943997728.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Stefan.&lt;/P&gt;</description>
      <pubDate>Tue, 17 Jan 2023 08:27:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-configure-ADC-using-MIMXRT1170-EVK/m-p/1583798#M7987</guid>
      <dc:creator>stefancinipeanu</dc:creator>
      <dc:date>2023-01-17T08:27:29Z</dc:date>
    </item>
  </channel>
</rss>