<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックHardware board is not reflecting in configuration parameter dialog box as i have installed the MBDT</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Hardware-board-is-not-reflecting-in-configuration-parameter/m-p/1560406#M7896</link>
    <description>&lt;P&gt;I have installed the model-based design toolbox for MPC5xx Microcontroller, but when I am going to configuration parameter block after modelling in MATLAB Hardware board is not reflecting. please help me to resolve this issue.&lt;/P&gt;</description>
    <pubDate>Mon, 28 Nov 2022 07:15:37 GMT</pubDate>
    <dc:creator>kuber2vedi</dc:creator>
    <dc:date>2022-11-28T07:15:37Z</dc:date>
    <item>
      <title>Hardware board is not reflecting in configuration parameter dialog box as i have installed the MBDT</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Hardware-board-is-not-reflecting-in-configuration-parameter/m-p/1560406#M7896</link>
      <description>&lt;P&gt;I have installed the model-based design toolbox for MPC5xx Microcontroller, but when I am going to configuration parameter block after modelling in MATLAB Hardware board is not reflecting. please help me to resolve this issue.&lt;/P&gt;</description>
      <pubDate>Mon, 28 Nov 2022 07:15:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Hardware-board-is-not-reflecting-in-configuration-parameter/m-p/1560406#M7896</guid>
      <dc:creator>kuber2vedi</dc:creator>
      <dc:date>2022-11-28T07:15:37Z</dc:date>
    </item>
    <item>
      <title>Re: Hardware board is not reflecting in configuration parameter dialog box as i have installed the M</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Hardware-board-is-not-reflecting-in-configuration-parameter/m-p/1578052#M7967</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/208813"&gt;@kuber2vedi&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I have installed the MPC57xx toolbox (version 3.2.0) and I was able to build an example out of the box without any modifications. Can you please provide more information about your problem (some screenshots can be useful)? What Matlab version do you use?&lt;/P&gt;
&lt;P&gt;Possible solution:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Remove the toolbox from the path (by executing the command &lt;STRONG&gt;mbd_mpc_path('remove')&amp;nbsp;&lt;/STRONG&gt;) then add it again (by executing the&amp;nbsp;&lt;STRONG&gt;mbd_mpc_path&lt;/STRONG&gt;).&lt;/LI&gt;
&lt;LI&gt;If you have installed another MBD toolboxes from NXP, you can try to remove them from matlab's path.&lt;/LI&gt;
&lt;LI&gt;Reinstall toolbox.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Bancila Sorin&lt;/P&gt;</description>
      <pubDate>Thu, 05 Jan 2023 14:50:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Hardware-board-is-not-reflecting-in-configuration-parameter/m-p/1578052#M7967</guid>
      <dc:creator>SorinIBancila</dc:creator>
      <dc:date>2023-01-05T14:50:04Z</dc:date>
    </item>
  </channel>
</rss>