<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Double to 16 bit fractional implementation using MLIB for S12ZVM in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Double-to-16-bit-fractional-implementation-using-MLIB-for-S12ZVM/m-p/1559515#M7892</link>
    <description>&lt;P&gt;Hi everybody,&lt;/P&gt;&lt;P&gt;i try to use the MBDT (Model Based Design toolbox) with the S12ZVM Controller. Is there any way to change from double values to 16 bit fractional implementation with just the blocks provided by "S12Z Automotive Math and Motor Control" Library? I am currently doing the recalculation with standard Simulink Blocks, but the execution time on the chip is very high for these block.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kind Regards,&lt;/P&gt;&lt;P&gt;Stefan&lt;/P&gt;</description>
    <pubDate>Thu, 24 Nov 2022 14:46:58 GMT</pubDate>
    <dc:creator>Stefan_9811</dc:creator>
    <dc:date>2022-11-24T14:46:58Z</dc:date>
    <item>
      <title>Double to 16 bit fractional implementation using MLIB for S12ZVM</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Double-to-16-bit-fractional-implementation-using-MLIB-for-S12ZVM/m-p/1559515#M7892</link>
      <description>&lt;P&gt;Hi everybody,&lt;/P&gt;&lt;P&gt;i try to use the MBDT (Model Based Design toolbox) with the S12ZVM Controller. Is there any way to change from double values to 16 bit fractional implementation with just the blocks provided by "S12Z Automotive Math and Motor Control" Library? I am currently doing the recalculation with standard Simulink Blocks, but the execution time on the chip is very high for these block.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kind Regards,&lt;/P&gt;&lt;P&gt;Stefan&lt;/P&gt;</description>
      <pubDate>Thu, 24 Nov 2022 14:46:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Double-to-16-bit-fractional-implementation-using-MLIB-for-S12ZVM/m-p/1559515#M7892</guid>
      <dc:creator>Stefan_9811</dc:creator>
      <dc:date>2022-11-24T14:46:58Z</dc:date>
    </item>
  </channel>
</rss>