<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックFTM module block in simulink</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/FTM-module-block-in-simulink/m-p/1539348#M7746</link>
    <description>&lt;P&gt;Hello i am trying a generate pwm signals from the FTM module block in simulink. The model is built without any errors but when i see the pwm outputs it is not what i expect it to be. the output is stuck at the initial duty cycle i entered in the block settings. i have attached the model .&lt;/P&gt;&lt;P&gt;Is the problem because of the sine wave sources? if it is then how can i incorporate sine wave source in the code generation.&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
    <pubDate>Tue, 18 Oct 2022 13:21:55 GMT</pubDate>
    <dc:creator>Sriram</dc:creator>
    <dc:date>2022-10-18T13:21:55Z</dc:date>
    <item>
      <title>FTM module block in simulink</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/FTM-module-block-in-simulink/m-p/1539348#M7746</link>
      <description>&lt;P&gt;Hello i am trying a generate pwm signals from the FTM module block in simulink. The model is built without any errors but when i see the pwm outputs it is not what i expect it to be. the output is stuck at the initial duty cycle i entered in the block settings. i have attached the model .&lt;/P&gt;&lt;P&gt;Is the problem because of the sine wave sources? if it is then how can i incorporate sine wave source in the code generation.&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
      <pubDate>Tue, 18 Oct 2022 13:21:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/FTM-module-block-in-simulink/m-p/1539348#M7746</guid>
      <dc:creator>Sriram</dc:creator>
      <dc:date>2022-10-18T13:21:55Z</dc:date>
    </item>
    <item>
      <title>Re: FTM module block in simulink</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/FTM-module-block-in-simulink/m-p/1542067#M7755</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The problem I found in your model is that the&amp;nbsp;&lt;STRONG&gt;Sample Time&amp;nbsp;&lt;/STRONG&gt;of the&amp;nbsp;&lt;STRONG&gt;PWM Generator&lt;/STRONG&gt; block is set too low. You can try to increase it so that each step has enough time to execute. You can try to use&amp;nbsp;&lt;STRONG&gt;S32Design Studio&lt;/STRONG&gt; &lt;STRONG&gt;for ARM&lt;/STRONG&gt; to debug your application. Place breakpoints in the step function&amp;nbsp;(&lt;STRONG&gt;&lt;SPAN&gt;svpwm_step)&lt;/SPAN&gt;&lt;/STRONG&gt;, found in &lt;STRONG&gt;'svpwm_mbd_rtw/svpwm.c&lt;/STRONG&gt;&lt;STRONG&gt;'&amp;nbsp;&lt;/STRONG&gt;and see if they are reached.&lt;/P&gt;
&lt;P&gt;Let me know if this helps you.&lt;/P&gt;
&lt;P&gt;Yours faithfully,&lt;/P&gt;
&lt;P&gt;Bancila Sorin-Ioanid&lt;/P&gt;</description>
      <pubDate>Fri, 21 Oct 2022 16:04:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/FTM-module-block-in-simulink/m-p/1542067#M7755</guid>
      <dc:creator>SorinIBancila</dc:creator>
      <dc:date>2022-10-21T16:04:24Z</dc:date>
    </item>
  </channel>
</rss>