<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: DEVKIT-MPC5744P random startup time of LED blinking test in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/DEVKIT-MPC5744P-random-startup-time-of-LED-blinking-test/m-p/1535505#M7732</link>
    <description>&lt;P&gt;Actually the board sometimes issued an error message which I can't remember. Some other postings here were suggesting this was due to a hardware error.&lt;/P&gt;&lt;P&gt;The board was eventually sent back.&lt;/P&gt;&lt;P&gt;Markus&lt;/P&gt;</description>
    <pubDate>Tue, 11 Oct 2022 08:58:57 GMT</pubDate>
    <dc:creator>mweiss</dc:creator>
    <dc:date>2022-10-11T08:58:57Z</dc:date>
    <item>
      <title>DEVKIT-MPC5744P random startup time of LED blinking test</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/DEVKIT-MPC5744P-random-startup-time-of-LED-blinking-test/m-p/1514029#M7642</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;with the mentioned devkit and MBDT in Simulink we have created a simple LED blinking test using a pulse generator. Downloading of *.elf built on an inhouse build server goes via S32 Design Studio. After flashing the device is powered off and on again, then:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;the LED is green but not at full brightness&lt;/LI&gt;&lt;LI&gt;after some random time 1s, 10s, or even longer the LED starts blinking&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;When we compile and run an example that comes with the S32 DS there is no such random time. ISR controlled LED blinking always starts right away.&lt;/P&gt;&lt;P&gt;Is there anything that can be done to avoid this random startup time?&lt;/P&gt;&lt;P&gt;Thx and best regards,&lt;BR /&gt;Markus&lt;/P&gt;</description>
      <pubDate>Tue, 30 Aug 2022 15:26:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/DEVKIT-MPC5744P-random-startup-time-of-LED-blinking-test/m-p/1514029#M7642</guid>
      <dc:creator>mweiss</dc:creator>
      <dc:date>2022-08-30T15:26:51Z</dc:date>
    </item>
    <item>
      <title>Re: DEVKIT-MPC5744P random startup time of LED blinking test</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/DEVKIT-MPC5744P-random-startup-time-of-LED-blinking-test/m-p/1535505#M7732</link>
      <description>&lt;P&gt;Actually the board sometimes issued an error message which I can't remember. Some other postings here were suggesting this was due to a hardware error.&lt;/P&gt;&lt;P&gt;The board was eventually sent back.&lt;/P&gt;&lt;P&gt;Markus&lt;/P&gt;</description>
      <pubDate>Tue, 11 Oct 2022 08:58:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/DEVKIT-MPC5744P-random-startup-time-of-LED-blinking-test/m-p/1535505#M7732</guid>
      <dc:creator>mweiss</dc:creator>
      <dc:date>2022-10-11T08:58:57Z</dc:date>
    </item>
  </channel>
</rss>