<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Code doesn't update after changing default channel in Simulink Block MBDT S32K3 in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Code-doesn-t-update-after-changing-default-channel-in-Simulink/m-p/1534698#M7728</link>
    <description>If I indeed the Bin, ELF file and modelName_ert_rtw folder the changed code can be generated and updated.&lt;BR /&gt;&lt;BR /&gt;Thank you</description>
    <pubDate>Mon, 10 Oct 2022 08:31:34 GMT</pubDate>
    <dc:creator>RobSpanjers</dc:creator>
    <dc:date>2022-10-10T08:31:34Z</dc:date>
    <item>
      <title>Code doesn't update after changing default channel in Simulink Block MBDT S32K3</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Code-doesn-t-update-after-changing-default-channel-in-Simulink/m-p/1533356#M7725</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;When I change the channel number from a block (DIO or PWM) and then generate and build a project, for the second time, the code doesn't update so the channel is the same as the first time I build the project.&lt;/P&gt;
&lt;P&gt;This happens in my own project as well as in the example projects.&lt;/P&gt;
&lt;P&gt;What should I change to get the code updated?&lt;/P&gt;
&lt;P&gt;I'm using:&lt;BR /&gt;-MATLAB 2021a&lt;BR /&gt;-MBDT S32K3 V1.2&lt;BR /&gt;-EB Tresos 28.2.0&lt;BR /&gt;-S32K344EVB-Q257&lt;/P&gt;</description>
      <pubDate>Thu, 06 Oct 2022 11:43:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Code-doesn-t-update-after-changing-default-channel-in-Simulink/m-p/1533356#M7725</guid>
      <dc:creator>RobSpanjers</dc:creator>
      <dc:date>2022-10-06T11:43:42Z</dc:date>
    </item>
    <item>
      <title>Re: Code doesn't update after changing default channel in Simulink Block MBDT S32K3</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Code-doesn-t-update-after-changing-default-channel-in-Simulink/m-p/1534675#M7727</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206113"&gt;@RobSpanjers&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;If the generated code does not get updated, I suggest you erase the artifacts from a previous build before regenerating the code with the new selections. Try deleting the &lt;EM&gt;modelName_ert_rtw&lt;/EM&gt; and &lt;EM&gt;slprj&lt;/EM&gt; folders, created next to the model, as well as the Simulink cache &lt;EM&gt;modelName.slxc&lt;/EM&gt; and rebuild your application.&lt;/P&gt;&lt;P&gt;Irina&lt;/P&gt;</description>
      <pubDate>Mon, 10 Oct 2022 07:59:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Code-doesn-t-update-after-changing-default-channel-in-Simulink/m-p/1534675#M7727</guid>
      <dc:creator>Irina_Costachescu</dc:creator>
      <dc:date>2022-10-10T07:59:18Z</dc:date>
    </item>
    <item>
      <title>Re: Code doesn't update after changing default channel in Simulink Block MBDT S32K3</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Code-doesn-t-update-after-changing-default-channel-in-Simulink/m-p/1534698#M7728</link>
      <description>If I indeed the Bin, ELF file and modelName_ert_rtw folder the changed code can be generated and updated.&lt;BR /&gt;&lt;BR /&gt;Thank you</description>
      <pubDate>Mon, 10 Oct 2022 08:31:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Code-doesn-t-update-after-changing-default-channel-in-Simulink/m-p/1534698#M7728</guid>
      <dc:creator>RobSpanjers</dc:creator>
      <dc:date>2022-10-10T08:31:34Z</dc:date>
    </item>
  </channel>
</rss>