<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックOne interupt multiple SM</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/One-interupt-multiple-SM/m-p/1524912#M7690</link>
    <description>&lt;P&gt;Hello all,&lt;BR /&gt;I am trying to create a SENT tx block which uses FlexIO, my idea is for a user to drag and drop the box and then in the box select timer and shifter, and output pin wrt to selected timer and shifter, for example, FLEXIOD2/3 are mapped to shifter1 and timer1 respectively and since there are multiple NXP pin associated to D3 pin with different mux I want the user to select this pin.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;But the problem I get is in parameter passing, and I can only have one instance of flexio interrupt so is there any way possible that interrupt is defined once, and then all the other blocks work as SM inside the interrupt.&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;JustMet&lt;/P&gt;</description>
    <pubDate>Tue, 20 Sep 2022 09:33:57 GMT</pubDate>
    <dc:creator>JustMet</dc:creator>
    <dc:date>2022-09-20T09:33:57Z</dc:date>
    <item>
      <title>One interupt multiple SM</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/One-interupt-multiple-SM/m-p/1524912#M7690</link>
      <description>&lt;P&gt;Hello all,&lt;BR /&gt;I am trying to create a SENT tx block which uses FlexIO, my idea is for a user to drag and drop the box and then in the box select timer and shifter, and output pin wrt to selected timer and shifter, for example, FLEXIOD2/3 are mapped to shifter1 and timer1 respectively and since there are multiple NXP pin associated to D3 pin with different mux I want the user to select this pin.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;But the problem I get is in parameter passing, and I can only have one instance of flexio interrupt so is there any way possible that interrupt is defined once, and then all the other blocks work as SM inside the interrupt.&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;JustMet&lt;/P&gt;</description>
      <pubDate>Tue, 20 Sep 2022 09:33:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/One-interupt-multiple-SM/m-p/1524912#M7690</guid>
      <dc:creator>JustMet</dc:creator>
      <dc:date>2022-09-20T09:33:57Z</dc:date>
    </item>
  </channel>
</rss>