<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MBD Toolbox generate S-Function in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBD-Toolbox-generate-S-Function/m-p/1519417#M7666</link>
    <description>&lt;P&gt;I am compiling a program for the MPC5744P. I have a model in Simulink which compiles well, but now I want to generate an S-Function automatically from a subsystem in this model. I run the process, but it always returns an error:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;Error: no configuration block for MPC57xx! Please add this block first.
Component:NXP MBD Toolbox | Category:Block error
An installed compiler was not detected. Certain simulation modes, as well as host-based coder builds require that a compiler be installed. Please install one of the supported compilers for this release as listed at:

http://www.mathworks.com/support/compilers/R2018a.html

MATLAB must be restarted after the compiler is installed.&lt;/LI-CODE&gt;&lt;P&gt;I have a configuration block at the top level of the model, but still gives this problem.&lt;/P&gt;&lt;P&gt;Has anyone had this problem? Any solutions to it?&lt;/P&gt;</description>
    <pubDate>Thu, 08 Sep 2022 13:59:51 GMT</pubDate>
    <dc:creator>mikel1</dc:creator>
    <dc:date>2022-09-08T13:59:51Z</dc:date>
    <item>
      <title>MBD Toolbox generate S-Function</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBD-Toolbox-generate-S-Function/m-p/1519417#M7666</link>
      <description>&lt;P&gt;I am compiling a program for the MPC5744P. I have a model in Simulink which compiles well, but now I want to generate an S-Function automatically from a subsystem in this model. I run the process, but it always returns an error:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;Error: no configuration block for MPC57xx! Please add this block first.
Component:NXP MBD Toolbox | Category:Block error
An installed compiler was not detected. Certain simulation modes, as well as host-based coder builds require that a compiler be installed. Please install one of the supported compilers for this release as listed at:

http://www.mathworks.com/support/compilers/R2018a.html

MATLAB must be restarted after the compiler is installed.&lt;/LI-CODE&gt;&lt;P&gt;I have a configuration block at the top level of the model, but still gives this problem.&lt;/P&gt;&lt;P&gt;Has anyone had this problem? Any solutions to it?&lt;/P&gt;</description>
      <pubDate>Thu, 08 Sep 2022 13:59:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBD-Toolbox-generate-S-Function/m-p/1519417#M7666</guid>
      <dc:creator>mikel1</dc:creator>
      <dc:date>2022-09-08T13:59:51Z</dc:date>
    </item>
  </channel>
</rss>