<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Errors compiling IMXRT1xxx GPIO polling model in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Errors-compiling-IMXRT1xxx-GPIO-polling-model/m-p/1518441#M7660</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm trying to compile a model with a GPIO input in polling mode for the MIMXRT1170-EVK and getting some errors when trying to generate the code. This model is based on the GPIO polling mode example included in the MBD Toolbox. In fact, it is the same model without the Stateflow+GPIO output part. I attached the diagnostic file and the project.&lt;/P&gt;&lt;P&gt;For your information, I'm using Matlab R2020b and NXP MBD Toolbox version is 1.3.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 07 Sep 2022 10:25:06 GMT</pubDate>
    <dc:creator>xabism</dc:creator>
    <dc:date>2022-09-07T10:25:06Z</dc:date>
    <item>
      <title>Errors compiling IMXRT1xxx GPIO polling model</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Errors-compiling-IMXRT1xxx-GPIO-polling-model/m-p/1518441#M7660</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm trying to compile a model with a GPIO input in polling mode for the MIMXRT1170-EVK and getting some errors when trying to generate the code. This model is based on the GPIO polling mode example included in the MBD Toolbox. In fact, it is the same model without the Stateflow+GPIO output part. I attached the diagnostic file and the project.&lt;/P&gt;&lt;P&gt;For your information, I'm using Matlab R2020b and NXP MBD Toolbox version is 1.3.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 07 Sep 2022 10:25:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Errors-compiling-IMXRT1xxx-GPIO-polling-model/m-p/1518441#M7660</guid>
      <dc:creator>xabism</dc:creator>
      <dc:date>2022-09-07T10:25:06Z</dc:date>
    </item>
    <item>
      <title>Re: Errors compiling IMXRT1xxx GPIO polling model</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Errors-compiling-IMXRT1xxx-GPIO-polling-model/m-p/1537431#M7739</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/204184"&gt;@xabism&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Please see this &lt;A href="https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Cannot-run-i-MXRT1060-examples-from-the-NXP-MBDToolbox-IMXRT1xxx/m-p/1187657#M5388" target="_self"&gt;post&lt;/A&gt;&amp;nbsp;for a fix for the problem you are seeing. What will need to do is to change the date time format in the Matlab preferences - this is explained in that post.&lt;/P&gt;
&lt;P&gt;Hope it helps,&lt;/P&gt;
&lt;P&gt;Alexandra&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 14 Oct 2022 02:17:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Errors-compiling-IMXRT1xxx-GPIO-polling-model/m-p/1537431#M7739</guid>
      <dc:creator>nxa11767</dc:creator>
      <dc:date>2022-10-14T02:17:03Z</dc:date>
    </item>
  </channel>
</rss>