<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックFlex CAN receiver</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Flex-CAN-receiver/m-p/1512862#M7630</link>
    <description>&lt;P&gt;I'm using NXP FlexCAN receive block in MATLAB Simulink, I want to receive data from BMS over CAN, the data is in floating format. But at end of the FlexCAN receive block, I'm getting physical value in decimal form ex: If I want a 3.2 data value then I'm getting 320, or If want 1.2 then getting 120. I also use a multiplier but the same problem. How can I resolve it?&lt;/P&gt;</description>
    <pubDate>Mon, 29 Aug 2022 04:52:49 GMT</pubDate>
    <dc:creator>saurabhkulkarni123</dc:creator>
    <dc:date>2022-08-29T04:52:49Z</dc:date>
    <item>
      <title>Flex CAN receiver</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Flex-CAN-receiver/m-p/1512862#M7630</link>
      <description>&lt;P&gt;I'm using NXP FlexCAN receive block in MATLAB Simulink, I want to receive data from BMS over CAN, the data is in floating format. But at end of the FlexCAN receive block, I'm getting physical value in decimal form ex: If I want a 3.2 data value then I'm getting 320, or If want 1.2 then getting 120. I also use a multiplier but the same problem. How can I resolve it?&lt;/P&gt;</description>
      <pubDate>Mon, 29 Aug 2022 04:52:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Flex-CAN-receiver/m-p/1512862#M7630</guid>
      <dc:creator>saurabhkulkarni123</dc:creator>
      <dc:date>2022-08-29T04:52:49Z</dc:date>
    </item>
  </channel>
</rss>