<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックFreemaster on CAN with other CAN blocks</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Freemaster-on-CAN-with-other-CAN-blocks/m-p/1511748#M7617</link>
    <description>&lt;P&gt;Is it possible to use Freemaster on CAN, and use the CAN Tx &amp;amp; Rx blocks on the same bus, from within Simulink ?&lt;/P&gt;&lt;P&gt;(our target ECU has no usb/uart interface - just CAN). I am using v4.2 of the MBDT&lt;/P&gt;</description>
    <pubDate>Thu, 25 Aug 2022 12:16:29 GMT</pubDate>
    <dc:creator>gmud1234</dc:creator>
    <dc:date>2022-08-25T12:16:29Z</dc:date>
    <item>
      <title>Freemaster on CAN with other CAN blocks</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Freemaster-on-CAN-with-other-CAN-blocks/m-p/1511748#M7617</link>
      <description>&lt;P&gt;Is it possible to use Freemaster on CAN, and use the CAN Tx &amp;amp; Rx blocks on the same bus, from within Simulink ?&lt;/P&gt;&lt;P&gt;(our target ECU has no usb/uart interface - just CAN). I am using v4.2 of the MBDT&lt;/P&gt;</description>
      <pubDate>Thu, 25 Aug 2022 12:16:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Freemaster-on-CAN-with-other-CAN-blocks/m-p/1511748#M7617</guid>
      <dc:creator>gmud1234</dc:creator>
      <dc:date>2022-08-25T12:16:29Z</dc:date>
    </item>
    <item>
      <title>Re: Freemaster on CAN with other CAN blocks</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Freemaster-on-CAN-with-other-CAN-blocks/m-p/1516991#M7651</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/204208"&gt;@gmud1234&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Unfortunately, you can't use the same CAN instance for Freemaster and Tx &amp;amp; Rx blocks. If your hardware allows it, you can use one CAN instance for Freemaster and another instance for sending/receiving CAN messages.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Bancila Sorin&lt;/P&gt;</description>
      <pubDate>Mon, 05 Sep 2022 10:37:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Freemaster-on-CAN-with-other-CAN-blocks/m-p/1516991#M7651</guid>
      <dc:creator>SorinIBancila</dc:creator>
      <dc:date>2022-09-05T10:37:35Z</dc:date>
    </item>
    <item>
      <title>Re: Freemaster on CAN with other CAN blocks</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Freemaster-on-CAN-with-other-CAN-blocks/m-p/1517005#M7653</link>
      <description>Thanks for the response.</description>
      <pubDate>Mon, 05 Sep 2022 10:58:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Freemaster-on-CAN-with-other-CAN-blocks/m-p/1517005#M7653</guid>
      <dc:creator>gmud1234</dc:creator>
      <dc:date>2022-09-05T10:58:25Z</dc:date>
    </item>
  </channel>
</rss>