<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックSENT Transmitter</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/SENT-Transmitter/m-p/1500925#M7589</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Hello Community,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I use the following code (see the attachment)&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;and made many types of block and configured tlc, the model is always building but I don't see any SENT signal on the oscilloscope&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I took this code and split the main into 2 one driver_setup() -&amp;gt; which contains all setup calls and one driver_action() -&amp;gt; which just contains while call; so that in the tlc file I can call setup only once and wait for trigger in action function.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Second I removed the ADC from the code took ADC config ADC Start from the NXP toolbox and took the data from it to the code same thing but in driver_action() I added a uint32_t Data variable in Parameter -&amp;gt; driver_action(uint32_t Data) and updated the tlc and my model to have one input port. it is built without error but with no result on the oscilloscope.&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;also, can I use all flexio pin simuntaniously for SENT Tx for example I use my block multiple times in Simulink and manipulate the data and then pass them to block; will all flexio pin transmit SENT signal w.r.t Data they recieved or is there some trick or something I am missing.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;BR /&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/203068"&gt;@JustMet&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 04 Aug 2022 08:20:26 GMT</pubDate>
    <dc:creator>JustMet</dc:creator>
    <dc:date>2022-08-04T08:20:26Z</dc:date>
    <item>
      <title>SENT Transmitter</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/SENT-Transmitter/m-p/1500925#M7589</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello Community,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I use the following code (see the attachment)&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;and made many types of block and configured tlc, the model is always building but I don't see any SENT signal on the oscilloscope&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I took this code and split the main into 2 one driver_setup() -&amp;gt; which contains all setup calls and one driver_action() -&amp;gt; which just contains while call; so that in the tlc file I can call setup only once and wait for trigger in action function.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Second I removed the ADC from the code took ADC config ADC Start from the NXP toolbox and took the data from it to the code same thing but in driver_action() I added a uint32_t Data variable in Parameter -&amp;gt; driver_action(uint32_t Data) and updated the tlc and my model to have one input port. it is built without error but with no result on the oscilloscope.&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;also, can I use all flexio pin simuntaniously for SENT Tx for example I use my block multiple times in Simulink and manipulate the data and then pass them to block; will all flexio pin transmit SENT signal w.r.t Data they recieved or is there some trick or something I am missing.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;BR /&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/203068"&gt;@JustMet&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 04 Aug 2022 08:20:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/SENT-Transmitter/m-p/1500925#M7589</guid>
      <dc:creator>JustMet</dc:creator>
      <dc:date>2022-08-04T08:20:26Z</dc:date>
    </item>
    <item>
      <title>Re: SENT Transmitter</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/SENT-Transmitter/m-p/1504028#M7603</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;I did some debugging and i found out that when i use clock divider function i see no output and when i disable it i just see clock output and not the SENT also i went a level in and found that selecting SIRC is causing the problem.&lt;/P&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;void&lt;/SPAN&gt; &lt;SPAN&gt;SCG_clock_dividers_setup&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;void&lt;/SPAN&gt;&lt;SPAN&gt;)&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;{&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;SCG&lt;/SPAN&gt;&lt;SPAN&gt;-&amp;gt;&lt;/SPAN&gt;&lt;SPAN&gt;RCCR&lt;/SPAN&gt;&lt;SPAN&gt; = &lt;/SPAN&gt;&lt;SPAN&gt;SCG_RCCR_SCS&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;1&lt;/SPAN&gt;&lt;SPAN&gt;) &amp;nbsp; &amp;nbsp; |&lt;/SPAN&gt;&lt;SPAN&gt; &amp;nbsp;/* SCS=2: System Clock Source is SIRC */&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;SCG_RCCR_DIVCORE&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;1&lt;/SPAN&gt;&lt;SPAN&gt;) |&lt;/SPAN&gt;&lt;SPAN&gt; &amp;nbsp;/* DIVCORE=1: Divided by 2, thus CORE/SYS_CLK frequency is 8 / 1 = 8MHz */&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;SCG_RCCR_DIVBUS&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;1&lt;/SPAN&gt;&lt;SPAN&gt;) &amp;nbsp;|&lt;/SPAN&gt;&lt;SPAN&gt; &amp;nbsp;/* DIVBUS=1: &amp;nbsp;Divided by 2, thus BUS_CLK frequency is 8 / 2 = 4MHz */&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;SCG_RCCR_DIVSLOW&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;2&lt;/SPAN&gt;&lt;SPAN&gt;);&lt;/SPAN&gt;&lt;SPAN&gt; &amp;nbsp; /* DIVSLOW=2: Divided by 3, thus FLASH_CLK is 8 / 3 = 2.67MHz */&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;SCG&lt;/SPAN&gt;&lt;SPAN&gt;-&amp;gt;&lt;/SPAN&gt;&lt;SPAN&gt;RCCR&lt;/SPAN&gt;&lt;SPAN&gt; |= &lt;/SPAN&gt;&lt;SPAN&gt;SCG_RCCR_SCS&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;6&lt;/SPAN&gt;&lt;SPAN&gt;);&lt;/SPAN&gt;&lt;SPAN&gt; &amp;nbsp; &amp;nbsp; &amp;nbsp;/* SCS=6: System Clock Source is System PLL */&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;/* DIVCORE=1: Divided by 2, thus CORE/SYS_CLK frequency is 80 / 1 = 80MHz */&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;/* DIVBUS=1: &amp;nbsp;Divided by 2, thus BUS_CLK frequency is 80 / 2 = 40MHz */&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;/* DIVSLOW=2: Divided by 3, thus FLASH_CLK is 80 / 3 = 26.6MHz */&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;Best regards,&lt;BR /&gt;JustMet&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Wed, 10 Aug 2022 13:28:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/SENT-Transmitter/m-p/1504028#M7603</guid>
      <dc:creator>JustMet</dc:creator>
      <dc:date>2022-08-10T13:28:53Z</dc:date>
    </item>
    <item>
      <title>Re: SENT Transmitter</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/SENT-Transmitter/m-p/1508236#M7608</link>
      <description>&lt;P&gt;Redefine Divocre Divbuss and Divslow and it work&lt;/P&gt;</description>
      <pubDate>Thu, 18 Aug 2022 11:52:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/SENT-Transmitter/m-p/1508236#M7608</guid>
      <dc:creator>JustMet</dc:creator>
      <dc:date>2022-08-18T11:52:08Z</dc:date>
    </item>
  </channel>
</rss>