<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)中的主题 S32K144 Model based design</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K144-Model-based-design/m-p/1482648#M7451</link>
    <description>&lt;P&gt;Hello ,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have sine cosine encoders for position sensing for pmsm foc. How do i replace the hall sensor part with the sine cosine encoder sensing part in the pmsm foc example .&lt;/P&gt;&lt;P&gt;Also what other blocks or parameters will be affected if i replace the hall sensor position sensing with sine cosine encoder. How should i estimate speed from the angle obtained from the sine cosine encoder.&lt;/P&gt;&lt;P&gt;I have attached the file which contains the sine cosine encoder model&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for the help.&lt;/P&gt;</description>
    <pubDate>Thu, 30 Jun 2022 11:16:07 GMT</pubDate>
    <dc:creator>Sriram</dc:creator>
    <dc:date>2022-06-30T11:16:07Z</dc:date>
    <item>
      <title>S32K144 Model based design</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K144-Model-based-design/m-p/1482648#M7451</link>
      <description>&lt;P&gt;Hello ,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have sine cosine encoders for position sensing for pmsm foc. How do i replace the hall sensor part with the sine cosine encoder sensing part in the pmsm foc example .&lt;/P&gt;&lt;P&gt;Also what other blocks or parameters will be affected if i replace the hall sensor position sensing with sine cosine encoder. How should i estimate speed from the angle obtained from the sine cosine encoder.&lt;/P&gt;&lt;P&gt;I have attached the file which contains the sine cosine encoder model&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for the help.&lt;/P&gt;</description>
      <pubDate>Thu, 30 Jun 2022 11:16:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K144-Model-based-design/m-p/1482648#M7451</guid>
      <dc:creator>Sriram</dc:creator>
      <dc:date>2022-06-30T11:16:07Z</dc:date>
    </item>
  </channel>
</rss>