<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックs32ct generate code error</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/s32ct-generate-code-error/m-p/1480985#M7446</link>
    <description>&lt;P&gt;It's something wrong happened when I tried to generate code with s32ct,fault details are shown in the figure.And it seems to be related to the can module.When I delete the can module, the code can be generated normally, and the fault occurs again after adding the module.&lt;/P&gt;&lt;P&gt;The version of s32ct is 1.4r，and it‘s installed automatically with mdbt (MBDToolbox_S32K3xx_1.1.0_20211220.mltbx)。And the chip is s32k344,footprint bga257.&lt;/P&gt;&lt;P&gt;I hope I can get some help,thanks very much.&lt;/P&gt;</description>
    <pubDate>Tue, 28 Jun 2022 07:02:29 GMT</pubDate>
    <dc:creator>ca_liu</dc:creator>
    <dc:date>2022-06-28T07:02:29Z</dc:date>
    <item>
      <title>s32ct generate code error</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/s32ct-generate-code-error/m-p/1480985#M7446</link>
      <description>&lt;P&gt;It's something wrong happened when I tried to generate code with s32ct,fault details are shown in the figure.And it seems to be related to the can module.When I delete the can module, the code can be generated normally, and the fault occurs again after adding the module.&lt;/P&gt;&lt;P&gt;The version of s32ct is 1.4r，and it‘s installed automatically with mdbt (MBDToolbox_S32K3xx_1.1.0_20211220.mltbx)。And the chip is s32k344,footprint bga257.&lt;/P&gt;&lt;P&gt;I hope I can get some help,thanks very much.&lt;/P&gt;</description>
      <pubDate>Tue, 28 Jun 2022 07:02:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/s32ct-generate-code-error/m-p/1480985#M7446</guid>
      <dc:creator>ca_liu</dc:creator>
      <dc:date>2022-06-28T07:02:29Z</dc:date>
    </item>
  </channel>
</rss>