<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)中的主题 MPC574x CCP Simulink CANape</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MPC574x-CCP-Simulink-CANape/m-p/1466936#M7362</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I would like to create application in Simulink and flash SPC574x using CCP and CANape tool and then access signals and parameters using CCP in CANape. I do not see any block regarding CCP in the library. Is it possible to generate .hex and .a2l and not flash with USB?&lt;/P&gt;&lt;P&gt;Is the workflow I mentioned possible in MBDT?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;</description>
    <pubDate>Tue, 31 May 2022 16:54:35 GMT</pubDate>
    <dc:creator>MateuszB</dc:creator>
    <dc:date>2022-05-31T16:54:35Z</dc:date>
    <item>
      <title>MPC574x CCP Simulink CANape</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MPC574x-CCP-Simulink-CANape/m-p/1466936#M7362</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I would like to create application in Simulink and flash SPC574x using CCP and CANape tool and then access signals and parameters using CCP in CANape. I do not see any block regarding CCP in the library. Is it possible to generate .hex and .a2l and not flash with USB?&lt;/P&gt;&lt;P&gt;Is the workflow I mentioned possible in MBDT?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;</description>
      <pubDate>Tue, 31 May 2022 16:54:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MPC574x-CCP-Simulink-CANape/m-p/1466936#M7362</guid>
      <dc:creator>MateuszB</dc:creator>
      <dc:date>2022-05-31T16:54:35Z</dc:date>
    </item>
    <item>
      <title>Re: MPC574x CCP Simulink CANape</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MPC574x-CCP-Simulink-CANape/m-p/1803286#M8833</link>
      <description>&lt;P&gt;I also want to know that&lt;/P&gt;</description>
      <pubDate>Wed, 07 Feb 2024 10:15:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MPC574x-CCP-Simulink-CANape/m-p/1803286#M8833</guid>
      <dc:creator>xiaoshida</dc:creator>
      <dc:date>2024-02-07T10:15:33Z</dc:date>
    </item>
  </channel>
</rss>